Part Number: AMC7836 Team,
My customer wants to set AMC7836 DAC output range to 0-5V, ADC input range to -12.5-12.5V at the same time, with AVCC=AVDD=5V, AVEE=AVSS=GND.
I want to double confirm if AMC7836 can support that. Thanks.
Part Number: AMC7836 Other Parts Discussed in Thread: ADS8028 , TINA-TI I has to evaluate if the bipolar an unipolar AMC7836 input channels are correctly driven in my design (output resistance and GBW of the driver opamp, Rf and Cf correctly defined). …
Part Number: AMC7836 Hi Team,
My customer is testing with AMC7836, and they found the GPIO pin was not pullup when powered the 3.3V-IOVDD.
The GPIO was actually pullup after powered the 5V-AVDD/DVDD.
Could you help explain this test performance?
BR …
Part Number: AMC7836 Hi Team,
I would like to inquire about the voltage range and time relationship of the LV ADC input pins of the AMC7836. For example, the manual states that when AVDD=5V, the max range of the LV_ADC pin is -0.3~5.3V. Is this referring…
Part Number: AMC7836
Hi Experts,
Good day! I am posting this on behalf of the customer.
Hi! We are students working on a master thesis project involving sending and reading analog data. We have been looking for a combined DAC/ADC module with requirements…
Part Number: AMC7836 Other Parts Discussed in Thread: AMC7904 , AFE10004 We are investigating a method of fast turn on and fast turn off the high power LDMOS transistors on the radio and I would like to know some information about the timing of the DAC…
Part Number: AMC7836 Team,
My customer has these two cases as below and need to check the AMC7836 DAC output status for these two cases. Note that the Vss is -8V in their system. Thank you!
Case #1: Bring up device normally -> IOVDD is floated after bring…
Part Number: AMC7836 Hi team:
My customer use AMC7836 in their DAS remote units by using two pcs AMC7836 for amplifier gate voltage read and write control, with a XILINX FPGA as the host and three slave devices hanging under the SPI bus: two AMC7836 (AD…
Part Number: AMC7836 Hi Team,
I have one question about the AMC7836 reset pin connection with MCU. I found in all reference design the Reset pin is pull up to IOVDD with ~kohm resistor. I want to know can I pull down the reset pin as below?
The advantages…
Part Number: AMC7836 Hi Team Now customer wanna use AMC7836 to complete the function show as below , Can you help to review if it is right of PIN assignment and configuration of AMC7836 show in Excel attachment. If not, Can you help show the right configuration…