Part Number: SN74LXCH8T245 Other Parts Discussed in Thread: AVCLVCDIRCNTRL-EVM
I like to check was there PCB board file available for this EVM AVCLVCDIRCNTRL-EVM ? Thanks.
Part Number: AVCLVCDIRCNTRL-EVM Hello Team,
I am thinking of ordering AVCLVCDIRCNTRL-EVM. Since the EVM is generic and supports both LVC and AVC, I am not sure if the EVM comes with any of these chips populated or should I order them separately.
Thank…
Part Number: SN74LXC1T45-Q1 Other Parts Discussed in Thread: AVCLVCDIRCNTRL-EVM , Hi,
In my current design I have a 3.3V source connected to VCCA and a voltage divider network connected to A that's roughly 3.3V. What is the pull down resistance on pin…
Hirotaka san,
I would suggest to consider the SN74LVC8T245 which is better in terms of the operating spec as compared to SN74LVCC3245A.
both are P2P replaceble and can be evaluated using the generic AVCLVCDIRCNTRL-EVM
John ,
www.ti.com/.../scea021a.pdf
The app note talks about the power up considerations for the device.
I would suggest considering the sn74LVC8t245 instead which works for across the power rails from 1.65 to 5.5V and is p2p with the lvcc4245a .
www…