Part Number: AWR2944P Hi,
SDK 4.7.1.4
CCS 20.1.0
SYSCFG 1.23
Port the driver example in AWR2X44P, check the syscfg, find the pin definition is for AWR2E44P, take I2C as example, shown in below figure, for I2C SDA can select pin T13/T19A19 which…
Part Number: AWR2944P
modify based on high end corner radar
radar_toolbox_3_30_00_06/source/ti/examples/Automotive_ADAS_and_Parking/high_end_corner_radar/src/demo/awr2x44p/mss/mss_main.c
Add a variable conditional_break, the if and debug log is…
Part Number: AWR2944P
1.flash in ccs debug image
2. ccs start and launch a configuration using awr2x44p
3.build a debug version and find a variable you may want to monitor like this:
here the forth (index 3) in gMmw_MCB.cqSigImgMonCfg with…
Part Number: AWR2944P Other Parts Discussed in Thread: SYSCONFIG , AWR2944 Tool/software: Hi,
I face an issue when I try to configure the ARM R5 on the AWR2944P with sysconfig. The following screenshot from the AWR2944 is not available for the AWR2944P…
Part Number: AWR2944P Other Parts Discussed in Thread: AWR2544 Tool/software: I
I want to debug AWR2944P application using CCS by when I create a .cxml target configuration file, gthe choic AWR2944P is nowhere to be found.
How to get it?
BR…
Part Number: AWR2944P Tool/software: Hello Expert,
I have some question for AWR_ADCOUT_CONF_SB.
The below discriptions from mmWave-Radar-Interface-Control.pdf:
"If the user desires 12 bit ADC output, then the digital front end (DFE) chain drops…
Part Number: AWR2944P Hi,
My customer debug on their own AWR2944ECO board, can connect R5, M4 through JTAG, but cannot connect DSP, same ccxml config can connect DSP, R5, M4 on AWR2944P. Customer also tried to send msg from R5 to DSP, but it is blocked…
Part Number: AWR2944P The routine for generating appimage has been provided in makefile_ccs_bootimage_gen. I would like to know if there are any related routines for generating the bin format. If there are, please let me know. Thank you.
Part Number: AWR2944P Hi,
I found below statement for AWR_MONITOR_TX0_PHASE_SHIFTER_CONF_SB.
Enable at least two phase settings to measure phase error and to apply threshold in reporting mode 1 and 2.
Does it mean that the min no. of…