Part Number: AWR6843ISK Other Parts Discussed in Thread: AWRL6432 , AWR6843 , AWR6843AOP , DCA1000EVM Hi Team,
recently i received AWR6843ISK and able to configure and also able to see the signal from 60GHz to 64GHz with 3 different configuration.
I have…
Part Number: AWR6843ISK I am using the parts listed in the title above and I am trying to figure out the max power consumption of both parts when they are turned on and active because I am trying to figure out the correct battery size needed to power…
Part Number: AWR6843ISK
Device used :AWR6843ISK- which has Tx antenna -3 ,Rx antenna -4
I have configured mmwavesensing estimator version_2.3.0 with system parameters as shown in the above screenshot and also done system calculation using the same scene…
Part Number: AWR6843ISK Other Parts Discussed in Thread: AWR6843 The awr6843 device has TX antenna= 3,Rx antenna =4.
It's mentioned that AZIMUTH FOV = +/- 60 deg and Elevation FOV =+/-15 deg.
Can you explain, how these values are calculated.
Kindly…
Part Number: AWR6843ISK Other Parts Discussed in Thread: MMWAVEICBOOST , , UNIFLASH , IWR6843 Hi There,
HW Config
MMWAVEICBOOST
Switch Configuration
S1.12: ON
S1.11: OFF
S1.10: OFF
S1.9: ON
S1.8: ON
S1.7: OFF
S1.6: OFF
S1.5: OFF
S1.4: ON
S1.3: OFF
S1…
Part Number: AWR6843ISK Other Parts Discussed in Thread: DCA1000EVM ,
Hello,
I am using the AWR6843ISK with the DCA1000evm and mmwave studio 2.1.1.0. When I try to connect to SPI, I keep getting a timeout error stating: [01:01:08] Status: Failed, Error…
Part Number: AWR6843AOPEVM
For measurement , I want to transmit a continuous wave at a single frequency .
We h ave mmW ave I C B OOST b oard a nd D CA1000EVM.
I w ould a ppreciate i t i f y ou c ould t ell m e h ow t o u se t hese.
B est regards.
…
Part Number: AWR6843AOPEVM Other Parts Discussed in Thread: AWR6843ISK , AWR6843 , AWR6843AOP
I would like to conduct a comparative experiment using AWR6843AOPEVM and AWR6843ISK .
Fo r t h is r e ason, w e w a nt t o ge t t h e r a w A D C d a ta f o r e a ch b …
Part Number: AWR6843ISK Other Parts Discussed in Thread: AWR6843 , AWRL6432 Hi, We're starting the development of an mmWave, autonomous (solar powered) radar device. We acquired the evaluation kit for the AWR6843 to start testing the FMCW techology capabilities…