Part Number: BEAGLEBN
Hi,
we use Buildroot for the Linux running on our Beaglebone Black. So far we have used the Buildroot version 2014.11 and were able to use both CAN interfaces. Now we decided to upgrade to the lates Buildroot LTS version 2019.02…
Part Number: BEAGLEBN
kernel = linux-rt-4.14.114+git:RobertCNelson/ti-linux-kernel-dev
cross compiler = arm-linux-gnueabihf-gcc
----------------------------------------------------------------------------------------------
Hi
I want to use the dmtimer…
Part Number: BEAGLEBN Dears:
Customer uses our BBB EVM to evaluate the performance of AM3358.
However, using eMMC failed, and pls. kindly provide the below website’s link?
Since these link can not download.
Part Number: BEAGLEBN
Tool/software: Linux
I have added the following configurations in my am335x-boneblack.dts file to enable uart4.
&am33xx_pinmux {
uart4_pins_default: uart4_pins_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x870, PIN_INPUT_PULLUP…
Part Number: BEAGLEBN
Tool/software: Linux
I have tried to get PWM working and am not having any success. I am using the TI SDK with a modified version of the am335x-boneblack.dts device tree (see below)
The PWM driver (ehrpwm1) probes correctly and appears…
Part Number: BEAGLEBN Hi,
On a BeagleboneBlack cluster (more than 32 beaglebone black wireless), when we start
up all the cards with the default mesh start scripts and 802.11s setup, after booting the 7th card it seems that the
wlcore/wl18xx (driver or…
Part Number: BEAGLEBN Tool/software: Linux Hi All ,
I am starting to learn Yocto & following the manual from the Yocto website
I have added meta-ti to yocto and create the images
Can team please provide some pointer to resolve the below error
or let…
Part Number: BEAGLEBN Hi, the datasheets specifies an "approximate 1 cycle" execution time of non-IO instruction, and "best case" 2 cycle GPIO read. What does the "approximate" term mean? That tight bit banging may actually have a jitter? What is the…
Part Number: BEAGLEBN Tool/software: Linux Hi,
I have a BBB flashed with the Arago pre-built image that comes with SDK Linux 05_01_00_11.
I have attached a USB sound card. It is correctly detected and I can play wav files with 'aplay'.
Now I am…