Part Number: BEAGLEBOARD-X15 Other Parts Discussed in Thread: TMDSEVM572X , Hi,
I have purchased 2 TMDSEVM572X modules, and one of the processors is damaged can I replace it with BEAGLEBOARD-X15, as all the components are the same can it be replaced with…
Part Number: BEAGLEBOARD-X15 Hi Experts, Good day. I need your help, Our customer is asking if the BEAGLEBOARD-X15 is compatible with Android 12? If yes, is there any instruction for a build update?
Thank you.
Regards, Josel Go
Part Number: BEAGLEBOARD-X15 When attempting to use the gdb_agent_console from CCS12.1.0 under Windows 10 with a board data file generated by a CCS test data connection for an AM62x connected to a XDS110 USB Debug. I tried a relative path or absolute path…
Part Number: BEAGLEBOARD-X15 Other Parts Discussed in Thread: AM5729 I have a Beaglebone AI (similar to the Beagleboard X15), and I understand that the Beaglebone AI-64 is coming out very soon.
I'm looking for examples that specifically show how to write…
Part Number: AM5728
Hi sir,
I am using Beagle board X15 and in dts file i changed in reg<2> in config files i selected all the things?
lcd0: display { compatible="gv,vidout", "panel-dpi"; label="vidout"; backlight…
Part Number: BEAGLEBOARD-X15 Other Parts Discussed in Thread: AM5728 , PMP I am using Buildroot to build kernel and rootfs using the kernel 4.9.147-ti-rt-r121 and uboot 2017.01. I enabled Gstreamer, QT5, and opencv in Buildroot. I could boot and run the…
Part Number: BEAGLEBOARD-X15 Hi sir,
I am using Beagleboard-x15 with ti-processor-sdk-linux-am57xx-evm-06.01.00.08 and u-boot 2019.1 and Linux 4.19.59 using,
Actually Beagle board x-15 of p16 connector is connected our custom fpga board from fpga to rugged…
Part Number: TPS659037 Other Parts Discussed in Thread: AM5728
Hello, there are several postings on the web regarding this issue, but the resolution is not clear.
The beagleboard X15 uses the TPS659037 PMIC and the AM5728 processor.
There is a button…
Part Number: BEAGLEBOARD-X15
Hi sir,
I am Ramachandra ,
I am using Beagleboard-x15 with ti-processor-sdk-linux-am57xx-evm-06.01.00.08 and u-boot 2019.1 and Linux 4.19.59 using,
Actually Beagle board x-15 of p16 connector is connected our custom fpga board…
Part Number: BEAGLEBOARD-X15
Hi,
SDK: ti-processor-sdk-android-am57xx-evm-06.03.00.106
Customer followed guide: https://www.ti.com/lit/an/spraco0/spraco0.pdf
Building source code:
export KERNELDIR=xxx/xxx/ti-processor-sdk-android-am57xx-evm-06.03.00…