Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: BLE-STACK Hi Ti teams:
This is the map file. And the heap size is 6655 Bytes.
When I download this fireware and it is failed to start.
Then I change setting to set the heap size to 34303…
Part Number: BLE-STACK Dear all member of the TI group,
Currently, I face with problem connection BLE between Central & peripheral is lost. It seems that LL_Feature_Req is ignored by peripheral.
Could al of you give me opinion or How to response LL_Feature_Req…
Part Number: CC2674R10
Hi,
Here is my use-case :
- I want to use the CC2674R10 in BLE only and then switch to Zigbee only in runtime.
- Once in Zigbee, I don't want the BLE stack / radio to have any impact on Zigbee and vice versa.
Questions :
-…
Part Number: CC2640R2F
Hi
We are trying to run BTOOL (C:\ti\simplelink_cc2640r2_sdk_5_30_00_03\tools\blestack\btool)
on BLE stack((simplelink_cc2640r2_sdk_5_30_00_03\examples\rtos\CC2640R2_LAUNCHXL\blestack\host_test) )
CC2640R2F launchpad but with…
Part Number: LP-CC2652RB Hi team,
I recently the simple_central example from the latest SDK to read the characteristic from another board. I see the GATT read function in the simple_central code. i was wondering if there is the example I can use to receive…
Part Number: CC2540 Other Parts Discussed in Thread: BLE-STACK Team,
Where can my customer locate older 1.3.x BLE stack versions for CC2540?
Thanks
Viktorija
Part Number: CC2340R5 Other Parts Discussed in Thread: SEGGER My customer is testing Segger RTT on CC2340R5 using J-Link. After integrating the RTT demo from Segger to CC2340 empty example, the RTT worked fine. However, after integrating the same code…
Part Number: CC2340R5 Hi,
As per the title, is it possible to use the BLE stack without needing to also use an RTOS?
I found this older thread which indicated that the RTOS is required but I wanted to just double check to understand what the options are…
Part Number: CC2642R-Q1
We are using the Simple Peripheral example code with all default parameters- the device is continuously advertising
We are measuring the current consumption of board by using voltage drop across a 100R series resistor
We are seeing…