Part Number: CC1352P Other Parts Discussed in Thread: SYSCONFIG
The documentation says the custom RF module in sysconfig allows the user full flexibility in choosing PHY settings but the exact consequences and limitations are not clearly defined.
What…
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: BLE-STACK Hi Ti teams:
This is the map file. And the heap size is 6655 Bytes.
When I download this fireware and it is failed to start.
Then I change setting to set the heap size to 34303…
Part Number: BLE-STACK Dear all member of the TI group,
Currently, I face with problem connection BLE between Central & peripheral is lost. It seems that LL_Feature_Req is ignored by peripheral.
Could al of you give me opinion or How to response LL_Feature_Req…
Part Number: CC2674R10
Hi,
Here is my use-case :
- I want to use the CC2674R10 in BLE only and then switch to Zigbee only in runtime.
- Once in Zigbee, I don't want the BLE stack / radio to have any impact on Zigbee and vice versa.
Questions :
-…
Part Number: Z-STACK-ARCHIVE Other Parts Discussed in Thread: Z-STACK I am currently having troubling running the Z-Stack Linux Gateway Installer from the Z-Stack Archive website. I have tried running it on a Linux system with a 32-bit ARM processor, in…
Part Number: CC2640R2F
Hi
We are trying to run BTOOL (C:\ti\simplelink_cc2640r2_sdk_5_30_00_03\tools\blestack\btool)
on BLE stack((simplelink_cc2640r2_sdk_5_30_00_03\examples\rtos\CC2640R2_LAUNCHXL\blestack\host_test) )
CC2640R2F launchpad but with…
Part Number: LP-CC2652RB Hi team,
I recently the simple_central example from the latest SDK to read the characteristic from another board. I see the GATT read function in the simple_central code. i was wondering if there is the example I can use to receive…
Part Number: CC2340R5 Other Parts Discussed in Thread: SEGGER My customer is testing Segger RTT on CC2340R5 using J-Link. After integrating the RTT demo from Segger to CC2340 empty example, the RTT worked fine. However, after integrating the same code…
Part Number: CC2540 Other Parts Discussed in Thread: BLE-STACK Team,
Where can my customer locate older 1.3.x BLE stack versions for CC2540?
Thanks
Viktorija