Sebastian,
schaefer1 said: Could you please give me a time horizon respectivly an information when this error will be fixed?
I don't have a timeline for a fix yet. I will update this thread as soon as this information is available.
Regards,
Rafa…
Part Number: CC2652R Dear Expert,
I am using BOOSTXL-AOA+CC2652
SDK version:5.2.00.52
I have 2 questions:
1. do you have a golden sample for BOOSTXL-AOA+CC2652 IQ csv file.
2. when I using BOOSTXL-AOA,i just modiy ble_user_config.c for ant truth table…
Part Number: BOOSTXL-AOA Hi TI expert
During AOA measurement, I encountered the problem that the extracted IQ data seems to be incompatible with our antenna switching sequence. Is this antenna switching sequence absolute? Is it possible that the antennas…
Hi,
Texas Instruments has always committed to provide the best products and tools to its customers and the BOOSTXL-AOA has been one of these tools. Originally released in 2018, this design has enabled engineers to evaluate Angle of Arrival (AoA) based…
Part Number: BOOSTXL-AOA Hello
Question 1. I have a LAUNCHXL-CC26X2R1, can this board connect with BOOSTXL-AOA? Or do I need to have LAUNCHXL-CC2640R2?
Question 2. If LAUNCHXL-CC26X2R1 can be connected to BOOSTXL-AOA, do I need to solder capacitors like…
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: CC1352R Dear Support members,
I am trying to do RTLS Visual Demo Connection AOA using two CC26X2R1 as locators, and both of them have BOOSTXL-AOA attached, and a CC1352R Sensor Tag as the…
Part Number: BOOSTXL-AOA Hello, I'm trying to use Bluetooth mesh with LaunchXL-AOA + BoostXL-AOA.
When I tried Bluetooth mesh with internal antenna to internal antenna, the transmitting distance was more than 80m.
But, if I tried with BoostXL-AOA…
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: CC1352R Dear Support members.
I am trying to do AOA using 2 CC26X2R1 and 1 CC1352R Sensor Tag without BOOSTXL-AOA.
1- Is it possible?
2- If (1) is possible, is there a demo of that on SDK?
…
Part Number: BOOSTXL-AOA Dear Community,
I have a couple questions regarding the LAUNCHXL-CC26X2R1 & BOOSTXL-AOA:
1. If I have those 2 as a receiver set, hooked up to a laptop, to display values & directions (like a compass) on a selfmade GUI (from…
Hi Eric,
The amount of IQ samples stored in rtls_aoa_iq_with_rtls_util_export_into_csv will depend of the number of CTEs sampled and the number of IQ samples extracted from each CTE.
To increase the number of CTE received, the only solution is to reduce…