I have used the "Dual Axis Servo Drive" example from the "C2000Ware_MotorControl_SDK_4_02_00_00".
As described in my initial post, I think I have made all the necessary changes to run the BOOSTXL-DRV8301.
Since my initial post, I have gotten closer…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: DRV8301 , LAUNCHXL-F28069M Dear TI, on page 2 of the BoostXL-DRV8301 Quick Start Guide and on page 4 of BoostXL-DRV8301 Hardware User's Guide, the drawing shows the DRV8301 connected to Launchpad…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE , CCSTUDIO I installed the instaspin universal Gui and it will not run past the l"loading application"screen.
Running Win 10 and copied the .out file to the directory.
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE How a c2000 uC is synching the ADC samples to make sure it is sampling when the low side fet is on? I am following lab guides and foc guides. There is no mention of how adc is synching…
Part Number: BOOSTXL-DRV8301 Hi Team,
Having issues getting MOSFETs to PWM on BOOSTXL-DRV8301 while connected to J5, J6, J7, J8 of LAUNCHXL-F28377S. Using Matlab Simulink to program in LAUNCHXL-F28377S. MOSFETs does not switch for channels PWM2A/B,…
Part Number: LAUNCHXL-F28069M Hi Team,
a PMSM motor with parameter:
pole pairs = 10
rate speed = 180RPM
rate voltage = 36V
Rs = 5.0R
Stator inductance = 27mH
Time constance = L/R = 5.4mS
The customer use lab02b to test the RoverL and Rs…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: LAUNCHXL-F28027F , , TIDA-00735 , TIDA-00643 , MOTORWARE Hello, I am trying to develop an esc for bldc sensorless motors with speeds between 8000 and 12000 rpm I have selected for this application…
Part Number: TMDSCNCD28069MISO Other Parts Discussed in Thread: BOOSTXL-DRV8301 Hi Team,
According to 2.1 Overview of user guide below, TMDSCNCD28069MISO can be paired with BOOSTXL-DRV8301.
But after checking the picture of both I can't find how they…
Part Number: LAUNCHXL-F280049C Other Parts Discussed in Thread: BOOSTXL-DRV8301 , , DRV8301 , DRV8320 , BOOSTXL-DRV8320RS
Hello,
I would like to use the BoostXL-DRV8301 (Rev B) on a LaunchXL-F280049C (Rev B).
In the software, I can see switches…
The motor can run at low speed without load on the BOOSTXL-DRV8301, but the the BOOSTXL-DRV8301 can't run the motor up to a high speed limit to the maximum dc bus.
Please take a look at the InstaSPIN lab guide (instaspin_labs.pdf) in the folder of motorWare…