Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: DRV8301-69M-KIT , LAUNCHXL-F280049C , TMS320F280049C , CONTROLSUITE , LAUNCHXL-F28027 , DRV8301 , DRV8343H-Q1EVM , BOOSTXL-DRV8323RH , LAUNCHXL-F280025C I need to integrate the BLDC motor drive…
Part Number: BOOSTXL-DRV8301 Hello everyone. I've got a question on a BOOSTXL-DRV8301 users. As far as I see, this driver is designed to handle current value up to 10A. What if I want to increase the current handling capability? Is it a matter of replacing…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: LAUNCHXL-F28069M ,
Hello, I have a tiny BLDC motor with 6 poles, a stator inductance of 30 uH, and series resistance of 0.8 ohms. It is an outrunner typically used in drones.
I am using…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE Tool/software: Code Composer Studio Hi there,
I want to base a BLDC generator design on the BOOSTXL-DRV8301 and F28069M launchpad combo. A lot of the TI information talks about…
Part Number: TMS320F28069M Other Parts Discussed in Thread: DRV8301 , BOOSTXL-DRV8301 , Hello, I am developing our motor control hardware using the TMS320F28069M and a BoostXL-DRV8301 boost board. I see that from the DRV8301 datasheet that if 3.3V is…
Part Number: BOOSTXL-DRV8301
Hello,
I am trying to power the motor driver through a 22.2v battery.
and this BOOSTXL-DRV3801 has input power up to 24v.
When the battery is fully charged, the battery voltage is a little over 25v, is that ok? Considering…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE Hello, I have been working on running a hobby motor ( Amazon.com: HobbyStar 550 Brushless Sensorless Motor, 4-Pole, 4300KV, 5.0mm Shaft, for 1/10 RC Short Course Truck : Toys & Games…
Part Number: BOOSTXL-DRV8301 Hello Team,
My customer is trying to power a 48V motor with this system. The datasheet for the DRV8301could handle up to 60V, however, the BOOSTXL-DRV8301 only handles 6-24V. Can you share with us why it is limited to that…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: DRV8301 , MOTORWARE Dear sir,
REcently I got the LAunch pad and BoostXL DRV8301. I have to drive SRM Motor. But there was no communication between Launch pad and Boostxl chip.
Except…