Part Number: BOOSTXL-DRV8320RS Hi Team,
VM voltage and Enable pin is good.
Do you have any idea or suggestion regarding Error -1044 & -1156?
Thanks!
Simon
This examples uses the on-chip PGA, you may take a look at the RTM of the F28004x to change the configuration code for PGA in hal.c, and then change the ADC_FULL_SCALE_CURRENT according to the gain of the PGA you used.
SeungGeun Yang said: in this case…
Part Number: BOOSTXL-DRV8320RS Hi everbody,
I'm using a BOOSTXL-DRV8320RS dev board.
When I supply the board (24V) I can measure a voltage peak on the output of buck regulator, and after a few milliseconds, I have my regulated voltage.
What do…
Part Number: BOOSTXL-DRV8320RS Other Parts Discussed in Thread: LAUNCHXL-F280049C Hi Team,
I'm writing this E2E thread for my customer, they using our BOOSTXL-DRV8320RS + LAUNCHXL-F280049C and successful to control a BLDC motor by Code Composer Studio…
Johannes Visser said: The motor is 15V 1,5A 1 pole pair PMSM (see above), RS=8Ohm, Ls_d = Ls_q = 30µH (measured with an LRC meter)
Since the motor is a low inductance motor, you need to use a higher PWM frequency like 45kHz as the settings below in…
Part Number: BOOSTXL-DRV8320RS Other Parts Discussed in Thread: LAUNCHXL-F280049C
Does the EVM BOOSTXL-DRV8320RS include a motor? if not can you recommend one?
Thanks,
Part Number: BOOSTXL-DRV8320RS Other Parts Discussed in Thread: LAUNCHXL-F280049C , Hi Everyone!
I've used the LAUNCHXL-F280049C and BOOSTXL-DRV8320RS to control small PMAC motors before without issue. I'm trying to control a small BLDC for the first…
Part Number: BOOSTXL-DRV8320RS Hello,
I am working with DRV8320RS EVM board.
The problem I have at the moment is that the motor runs only upto 3A. I want to test the motor to the max 15A phase current.
Do anyone here know how I can change the current…
Part Number: BOOSTXL-DRV8320RS Hi Team,
Customer is encountering overcurrent in his test, below is the details.
"With Lab03 I run into an over current error right after I activate the Lab by setting motorVars.flagEnableSys and motorVars.flagRunIdentAndOnLine…
Part Number: BOOSTXL-DRV8320RS Hi
I try to use MotorSDK to control my motor and it is in good condition.
But I want to detect 300RPM~1450RPM torque motor, but when the motor is disturbed, the robustness is very poor. Is there any good way to robustness…