Part Number: BOOSTXL-DRV8305EVM Other Parts Discussed in Thread: DRV8305 , BOOSTXL-DRV8320RS , TMS320F280049C , LAUNCHXL-F280049C , DRV8323 , DRV8320 Tool/software: Code Composer Studio Dear team,
This is regarding the usage of DRV8305 EVM with 280049C…
?? ? said: 1. Is this project also a motor identification error?
You need to configure the parameters for identification and use a higher PWM and control frequency if the motor is a low inductance motor, such as 45KHz PWM frequency, 15kHz control frequency…
Part Number: BOOSTXL-DRV8320RS Other Parts Discussed in Thread: C2000WARE Hi Team,
My customer is development the motor control system, and they use below two our EVM in test design stage.
DSP LaunchPad - F280049C ( https://www.ti.com/tool/LAUNCHXL…
jgerhardy said: Why two defines for the same thing?
There are two sites for connection the BoosterPak to LaunchXL-F280049C. Using site 1 is the default setting.
jgerhardy said: Is this the right setting?
Right. It's for installing the BoosterPak…
Part Number: BOOSTXL-DRV8320RS Other Parts Discussed in Thread: LAUNCHXL-F280049C , , DRV8320 1)
The default value of USER_ADC_FULL_SCALE_CURRENT_A is:
//! \brief Defines the maximum current at the AD converter //! BOARD_BSXL8320RS_REVA, Gain=12 …
Part Number: BOOSTXL-DRV8320RS Other Parts Discussed in Thread: TMS320F28379D , , DRV8323 , TMDXIDDK379D , C2000WARE
Tool/software: Code Composer Studio
Dear ti community,
we are developing bldc application using boostxl-drv8320rs with tms320f28379d…
Part Number: BOOSTXL-DRV8320RS Other Parts Discussed in Thread: LAUNCHXL-F280049C , DRV8320 BOOSTXL-DRV8320RS + LAUNCHXL-F280049C to run the motor drive Total power supply: 36V lithium battery power supply:
1.The 5-V, 3.3-V power supply on the LAUNCHXL…
The PWMDAC function can't be used on the LuanchPad-F28049 with BOOSTXL-DRV8320RS since there is no circuit for PWMDAC on the LuanchPad-F28049. It's just for the high voltage kit with F280049C control card. Please ignore this PWMDAC function.