Part Number: BOOSTXL-DRV8323RS Other Parts Discussed in Thread: MSP-EXP430F5529LP , DRV8323 , MCT8316Z Hello,
I'm looking for a way to use the BOOSTXL-DRV8323RS at a constant speed with varying loads. The BOOSXL_DRB823X GUI used with the MSP-EXP430F5529LP…
Part Number: BOOSTXL-DRV8323RS Hi Team,
The customer wants to know whether it is feasible to add inductors to the three phases of the brushless DC motor to reduce the slope and amplitude of the drive current, thereby reducing the temperature rise of the…
Part Number: TMS320F2800157-Q1 Other Parts Discussed in Thread: BOOSTXL-DRV8323RS , LAUNCHXL-F2800157 我想使用这两个套件 LAUNCHXL-F2800157 +BOOSTXL-DRV8323RS组合起来,实现低压电机的无传感FOC控制。但是没有找到2800157的launchpad 与 BOOSTXL-DRV8323RS组合使用 的设置方式的指导手册(主要是关于
LAUNCHXL-F2800157 的设置 )。有知道的吗…
Part Number: BOOSTXL-DRV8323RS Hi Team,
Customer just connects the BOOSTXL-DRV8323RS evaluation board to the BLDC motor without connecting the MCU. Could he make the motor rotate by rotating the encoder in the picture?
Regards,
Annie
Part Number: BOOSTXL-DRV8323RS Other Parts Discussed in Thread: LAUNCHXL-F28069M , Hello
I am able to tune 2 different motors on single Controller.
(BOOSTXL-DRV8323RS + LAUNCHXL-F28069M)
Speed and Current Controllers are properly tuned.
Resistance and Inductance…
Part Number: BOOSTXL-DRV8323RS While spinning a BDLC motor in 1x PWM mode, I keep getting a "VOLTAGE" fault in the GUI window (where the speed and direction is set), which causes the motor to stop. To be clear, this is NOT an Overvoltage, Undervoltage…
Part Number: BOOSTXL-DRV8323RS Other Parts Discussed in Thread: LAUNCHXL-F280039C , , MSP430F5529 , LAUNCHXL-F28379D Is BOOSTXL-DRV8323RS compatible with LAUNCHXL-F280039C?
Hi Danny,
Danny Chan said: Can you please help to confirm if little resistor e.g. 10 ohm is needed in GH and GL line to prevent oscillation damage MOSFET ?
Please refer to the datahseet
Danny Chan said: also for the resistor C1, is it connect to board…
Part Number: BOOSTXL-DRV8323RS Other Parts Discussed in Thread: C2000WARE , DRV8323 Hello,
I am trying to set up the motor driver to work with the launchpadxl-f280049C. What are the steps needed to port the example project from the msp430 to the f280049C…
Part Number: BOOSTXL-DRV8323RS Hi Team,
Testing with the DRV8323RS development board and it's found that there is a ramp in the gate waveform of the 3-phase lower leg. The gate voltage is as high as 20 V when the lower leg is turned on and then slowly…