Part Number: LP-MSPM0L1306 Hi,
Quick question is the BOOSTXL Sensor pack ( https://www.ti.com/tool/BOOSTXL-SENSORS) compatible with the M0? Or is it primarily meant for the MSP430?
Thank you!
Part Number: BOOSTXL-SENSORS Hi
Trying to run BOOSTXL-SENSORS_GUI+ET. When selecting File->Program Device I get the error "Error Configuring Debug Server: error = operation was aborted"
HW:BOOSTXL-SENSORS + cc1310 launchpad
1. BOOSTXL…
Part Number: BOOSTXL-SENSORS
I have the MSP430FR6989 MCU and BOOSTXL-BASSENSORS connected. I believe the booster pack just needs to be on top of the MSP430 Launchpad as they are both 40 pin compatible. Assuming I have these connected correctly, I tried…
Part Number: BOOSTXL-SENSORS
Hey!
We are developing an Autonomous Mobile Robot. As per our design, an IMU sensor is placed between two motors that are in a differential drive setup.
The IMU sensor that we are presently using is heavily affected by EMF…
Hi Danny,
Danny Chan said: with FAST and HALL both enabled, by default I should run either HALL or FAST right ?
Yes. If you have both FAST and HALL enabled, the estimator mode is FAST or HALL depending on variable "obj->estimatorMode".
The…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: SIMPLELINK-CC13X0-SDK , CC1310 Hello Community,
I have purchased CC1310 LaunchXL and BoostXL-Sensors (Sensors BoosterPack Plug-In Module) and was working on these TI-Tools I was able to execute…
Part Number: BOOSTXL-SENSORS Dear team,
1. Can BOOSTXL-SENSORS work with F28379D LaunchPad to collect angle signals based on simulink?
2. Can you please help provide the algorithm for converting the Bosch BMI160 output signal into an angle in BOOSTXL-SENSORS…
Part Number: BOOSTXL-EDUMKII Other Parts Discussed in Thread: OPT3001 , MSP432E401Y
Hi,
I recently purchased the boosterpack BOOSTXL-EDUMKII. I have paired it with my MSP432P401R launchpad.
When I run the light sensor demo which ships with the SDK …
Part Number: BOOSTXL-EDUMKII Hi,
I recently purchased the boosterpack BOOSTXL-EDUMKII. I have paired it with my MSP432P401R launchpad. When testing the setup I see that the temperature sensor demo which ships with the SDK (boostxl_edumkii_temperature_msp432p401r…
Part Number: BOOSTXL-3PHGANINV Other Parts Discussed in Thread: C2000WARE , SYSCONFIG Hello,
We are currently trying to modify the existing project located in :
"C:\ti\c2000\C2000Ware_MotorControl_SDK_4_00_00_00\solutions\boostxl_3phganinv\f2837x\ccs\sensored_foc…