Part Number: BOOSTXL-TUSS4470 Hello,
How do I know which threshold value to use? What parameters should I use to know the threshold value?
Thank you,
Julia
Part Number: BOOSTXL-TUSS4470 Other Parts Discussed in Thread: MSP-EXP430F5529LP , Hi,
I am using the BOOSTXL-TUSS4470 connected to MSP-EXP430F5529LP. The power mode is set to external only with the jumper position J6 3-4 short and J6 1-2, 5-6, J8 1-2,…
Part Number: BOOSTXL-TUSS4470 Other Parts Discussed in Thread: LAUNCHXL-F2800137 , MSP430F5529 , ENERGIA , TUSS4470 , Can F2800137 LaunchPad be used as a host board to interface with the TUSS44x0 EVM and control its operation? Can you help to give me an example…
Part Number: BOOSTXL-TUSS4470 Hi,
I would like to know if it is possible to use two transducers using only one BOOSTXL-TUSS4470 board. And what modification should I make to BOSSTXL-TUSS4470, if such a change is possible?
I am using MSP-EXP430F5529 LaunchPad…
Part Number: BOOSTXL-TUSS4470 Other Parts Discussed in Thread: MSP-EXP430F5529LP , TUSS4470 , TDC7201 , TDC7200 , TDC1000 I have two BOOSTXL-TUSS4470 I need to link these to be master and slave, as to take a ToF measurement between PMMA transducers?
The manual…
Part Number: BOOSTXL-TUSS4470 Other Parts Discussed in Thread: TUSS4470 , MSP-EXP430F5529LP Hello E2E Experts,
Good day.
I cannot find the "En" checkbox or "Master" checkbox anywhere in the TUSS4470 EVM GUI. Please help me to find it.…
Part Number: BOOSTXL-TUSS4470 Other Parts Discussed in Thread: TUSS4470 Hello,
I just realized BOOSTXL-TUSS4470 has a pin called FLT and if this pin is like in the function block diagram, it is a pin that will very useful for me.
But I can't find any…
Part Number: BOOSTXL-TUSS4470 Other Parts Discussed in Thread: MSP-EXP430F5529LP , UNIFLASH Hello,
I've recently purchased a BOOSTXLTUSS4470 and MSP-EXP430F5529LP, I've downloaded the GUI and stacked them up as in the guide. The GUI says no TUSS4xx0 device…
Part Number: BOOSTXL-TUSS4470
I was using the EVM GUI for 2 weeks.There was no problem with it. After that I tried some c code in Code Composer Studio. Now I'm back to using the gui again but I can not connect the hardware.
So I have the same issue…
Part Number: BOOSTXL-TUSS4470 Hello, I'm trying capture echo signal with two 1Mhz transducers on two sides on 9cm water tank. I was using just one transducer but blind zone was longer than echos returning time. In my application i must measure echos frequency…