Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: MSP432E401Y Good day I have a question regarding the BP-DAC11001EVM. I wanted to try out the built-in DAC from the board. However, I have not found out which file is needed for the MSP432E401Y…
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: ENERGIA Hello, I'm trying write a control loop in python using a Real-time operating system (RTOS). I want output voltage setpoints to a DAC at ~10kHz. The voltage outputs are single values…
Part Number: BP-DAC11001EVM Hello everyone !!
I'm doing a Bachelor Thesis on the control of a special device with a DAC so I wanted to first test the controlling of the DAC with my Arduino MKR Vidor 4000 board.
I have tested the SPI communication…
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: DAC11001B Hi there,
We are debugging DAC11001 for our project. we use EXP432E401Y MCU for controlling DAC11001 output. But we do not have the EXP432E401Y original code/project, could you please…
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: DAC11001B Hi Team,
Can you explain what is the purpose of the U10 circuitry below?
Thank you,
Regards,
Marvin
Part Number: BP-DAC11001EVM I am designing a pcb and would like to place the DAC but for this I require design files of the following board: BP-DAC11001EVM can you please assist.
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: REF6250
Hi there,
I have bought DAC11001EVM and MSP-432E401Y demo. The power-up sequence and value as below.
VCC: +9V
VSS: -9V
VDD: +5V ( same power with VIO )
VIO: +5V
VREF_PWR : +5V…
Part Number: BP-DAC11001EVM
Hi there,
Please help to check if below SPI WRITE process is right. ( using GUI write 01H register 00FA00 ), Also, please help to let me know the read process.
When I send write 01H register for 00FA00 data, I set up the…
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: MSP-EXP432E401Y
Hi TI Team
I have a related question:
So I bought the same Kit (BP-DAC11001EVM and MSP-EXP432E401Y) and I got stuck in the same error as Allison Ma.
( (+) BP-DAC11001EVM: BP…