Part Number: BQ21061 Hello There,
1. Is there a SPICE MODEL for BQ21061 on TI website? 2. Can I simulate the above part? If yes, shall I download TINA?
All comments are welcome.
Thanks,
Raymond
Part Number: BQ21061 Hello E2E Team,
I am having problem using BQ21061 single-cell charger; usually, no problem with TI Parts. This is my first-time in years!
Please share your experience if anyone has used this device before and seen similar problems…
Part Number: BQ21061 Hello,
I am using bq21061 to charge a single Li-ion cell.
Do I need to use a FG part, like bq27546, to check on the charger IC bq21061?
For your information, there is a MCU that I can use to monitor the behavior of the battery…
Part Number: BQ21061 Dear,
I would like to know if we can routing out the /INT pin of BQ21061 connecting this pin to NC1 and NC2 pins avoiding via-in pad solution. From your application note "Slua996" I understand that it is possible to routing out…
Part Number: BQ21061 Hi team,
In customer side we met a strange issue. Customer use BQ21061 and its TS function. They found that TS voltage is only 18mV, and charging can't work. After reading the register, STAT0=0x01, STAT1=0x00, STAT2=0x01, which…
Part Number: BQ21061 About TI battery charger BQ21061YFPR, I have the following questions during product validation. Kindly advise it. Thanks.
1、REF the datasheet “2b00 = PMID powered from BAT or VIN if present”, does it means:
if Vin present,the…
Part Number: BQ21061 Dears,
One of my customer is using the BQ21061 for a wearable device, and they want to have the status of Fast charger flag, seemed we do not have this status register? and if yes, is there a way to know the charger is in the…
Part Number: BQ21061 Other Parts Discussed in Thread: BQ25155 Hi team, customer decide to use BQ21061 based on recommendation and customer would like to implement the different charging current at different stage voltage. BQ21061 does not integrate ADC…