Part Number: BQ21061 Hi Ti Team,
I am using the I2C-Controlled charger IC and have two issues with the part:
1. As soon as I connect VIN of 4.5V, this voltage is present at PMID.
Is it possible to stop that while I am charging the battery?
2.…
Part Number: BQ21061 Hello Expert,
Could you help explain more details about tI2CRESET I 2C interface inactive reset timer 500ms? As the picture below, I can't find more in the datasheet. Thanks.
Part Number: BQ21061 Dear expert,
My customer is evaluating BQ21061. The input is 32mA@5V, input current will be too small to supply the system with normal power. The output is 1s Li-on battery and system load(I'm checking the system load current with…
Part Number: BQ21061 Hi. Is there any way(s) to detect if the device is in ship mode or not, by probing one of the pins?
I know no output is operational in ship mode. But is there some output that I can use that has a defined state, and/or that I can…
Part Number: BQ21061
Hi TI:
We are using bq21061 as our PMID for battery charging.
However we discovered that after battery is fully charged and the charge done flag is set. unpluging the charging USB cable and immediately pluging in back will clear…
Part Number: BQ21061 Hi,
I am considering using the BQ21061 device. I would like to ask the following questions about device behavior.
1.About MR function Is the following operation when waking up from Ship Mode? When the button is pressed (wake1…
Part Number: BQ21061 Hello Team,
I set Charger safety timer is 3H for a test after 3H charger stopped, but SAFETY_TMR_FAULT_FLAG is not set to 1. As figure below.
If we want to get the sign when safety timer expires, how to deal with this register…
Part Number: BQ21061 Other Parts Discussed in Thread: BQ25101 , BQ25120A , BQ25155 Hi team,
i need a single cell Li battery charger that has the following features/specs:
1. LED state of charge output feature.(to show the charge on battery)
2…
Part Number: BQ21061 Other Parts Discussed in Thread: BQ25155 Is it possible to increase BUVLO to above 3.0V? Further is this from the datasheet accurate? It seems strange that there are 3 settings for 3.0V and none that are higher
Part Number: BQ21061 Hello,
May I have your options on the question below, thanks.
Under multitasking, BQ21601 I2C communication error occurs, like NACK... how to reset in normal mode without power down?
Thanks.