Part Number: BQ24160 Other Parts Discussed in Thread: BQ500212A When using the IN source I see faults at just below 4.1V. About 75% capacity. My charge current is 300mA. It will charge for some number of seconds(3-20) then fault and repeat. The net effect…
Part Number: BQ24160 Hi,
What will be the USB input current setting of BQ24160 if:
1) The charger starts from an external DC adapter
2) The charger starts from USB, but without an active device at D+/D-
3) The charger start from USB, but there…
Part Number: BQ24160 Other Parts Discussed in Thread: BQ25890 Hello,community
I asked the following questions and got answers.
Regarding “it will allow current to flow from BAT to SYS in supplement mode as needed”, what is the state when the FET turns…
Part Number: BQ24160 Hello,
Now I'm investigating defective products that don't shift to recharging.
It seems that the safety timer is working for 6 hours after the battery is fully charged with 5V supplied from DC IN.
See attached figure, 1. Charging…
Part Number: BQ24160 Other Parts Discussed in Thread: BQ25601D , BQ25890 Hi,
I'd like to use BQ24160 in an application, where I would like to use USB for fast charging trough BQ24160, and use the USB for communication too. How can I connect the data…
Part Number: BQ24160 Other Parts Discussed in Thread: TUSB320 , BQ25601D Thanks for the response.
Block diagram shows TI charger IC for Type C connector. Here IC BQ24160 is shown ( I think we can use any charger IC with I limit >1.5A and USB support…
Part Number: BQ24160 Hello,
Currently I'm using BQ24160 in one of my designs. In status/Control Register, there are two indications in STAT_x bits, those are unclear to me.
000 - No valid source detected 110 - NA
What is the difference between these…
Part Number: BQ24160 Hi Jeff, We use the BQ24160 to design a car product. Connect the product to the cigarette lighter for charging. When Battery is charged to the 95%~100% range, The recharge voltage IN (4.58V) appears when the cigarette lighter connection…
Part Number: BQ24160 Hi sir,
Regarding to the BQ24160, when the DC power input is 5V and BQ24160 are broken by surge/ESD energy,
Could you tell us the internal of IC (for example MOS or dc/dc converter) are open or short?
It means that IN was opened…