Part Number: BQ24250C Other Parts Discussed in Thread: BQ24250 Dear team
The customer originally used BQ24250, but now they want to change e the solution to BQ24250 C , what should they pay attention to? If TI have a migration guide be provided?
Many thanks
…
Part Number: BQ24250 Other Parts Discussed in Thread: TUSB320 Can I use BQ24250C charger IC with USB Type C connector. The CC pins of USB Type C can be used for initial detection, so that host will supply 5V power to Charger IC.
In this approach also current…
Part Number: BQ24250C Other Parts Discussed in Thread: BQ27532-G1 , BQ24250 Hi,
We are using BQ24250C and BQ27532-G1 in our product.
We use Li-ion Battery of 8000mA (4 parallel batteries).
We charge the battery and it get to full charge and then the input…
Other Parts Discussed in Thread: BQ24250C Dears,
Is there the DSN file for BQ24250C available?
I cannot find on TI website.
If yes, please help to provide to me!
My email is: peter.tseng@arrowasia.com
Thanks.
Other Parts Discussed in Thread: TPS63020 , BQ24250C Hello all,
In my application, I'm using the bq24250c battery charger along with a buck-boost converter (TPS63020)
The TPS63020 buck-boost converter uses a 1.5uHy inductor.
I was wondering if I can…
Other Parts Discussed in Thread: BQ24250C Hello,
what should be the capacitor value connected to system load in schematic of bq24250c? and what is the system load exactly??
Other Parts Discussed in Thread: BQ24250C , BQ24250 Hello.
I have doubts about the behaviour of bq24250 and bq24250C:
bq24250
1.- If I put /CE pin HIGH the charge is disabled. I want to put this pin to a fixed HIGH level and start charging only via I2C…
Other Parts Discussed in Thread: BQ24250 Hi All,
I'm trying to prepare the NTC calculation tool by MS excel but the equations to calculate dividers for TS pin are a little bit complicated... I attached the tool but it's appreciated if you can share…
Other Parts Discussed in Thread: BQ24250C Hello~
In the page 30 of bq24250c's datasheet, Register #3 B[1:0] is described the EN1/EN0 pin status.
But, bq24250c does not have the EN0 pin. bq24250c just has EN2 pin instead of EN0.
Is the "EN1/EN0"…