Part Number: BQ24250EVM-150 Other Parts Discussed in Thread: BQSTUDIO , BQ25619 , BQ25618 , BQ25616 Hello,
It looks like bq2425x can't be managed by bqStudio. bq2425x chargers need HPA172 I2C to USB interface - plus the proper driver - to be programmed via…
Part Number: BQ24250EVM-150 Dear Sir,
I check functions of BQ24250EVM-150 .
When I disconnect the battery, The Vsys and Vbat become the rectangular wave form, 3.7V~4.2V, 15Hz.
And then,I tune the TS temp > THOT (V_Ts=1V) and the Vsys don't modulate.…
Part Number: BQ24250EVM-150 Other Parts Discussed in Thread: BQ24250C , BQ24250 Dear Sir,
I check functions of BQ24250EVM-150.
I don't use any SW to control the EVM ans set EN1=H, EN2=L.
Functions are OK when I connect the battery and Vin=5V.
When I…
Part Number: BQ24250EVM-150 Other Parts Discussed in Thread: BQ24250
We are using BQ24250 for large current. The chip on my first prototype board is hot and the one one this EVM board is cool. Can I have gerber file for BQ24250EVM board to reference? …
First I bought the bq24250EVM-150, and later I purchased the bq27532EVM-656. Is there anyway to use the USB interface adapter that cames along with the bq24250EVM-150 as a way to communicate with the second module, or I just need to purchase the EV2300…
Other Parts Discussed in Thread: BQ24250 , BQ24250EVM-150 I am using bq24250 and am experiencing a problem with Vbatreg clipping to 4.0V. This happens both in stand-alone and i2c mode
The value of Vbatreg in stand alone mode is always 4.0V (not 4.2 as expected…
Other Parts Discussed in Thread: BQ24250EVM-150 While following the recommended test procedure in the user guide of the BQ2425Xevm-150. I want to set up the battery emulator as mentioned in the figure 3 of user guide and I couldn't understand why you have…