Hi Aya,
We couldn't provide waveforms to you because of we have only 2 channel DSO. Anyway my issue is resolved after purchase the EVK module.
There are more than two difference found from EVK to datasheet.
I would like to thanks for your support.
…
Part Number: BQ24725A Other Parts Discussed in Thread: BQ24725 Hi Team,
BQ24725 have MPS MP2760 Trickle charge function? Or do you have other better suggestions?
When the battery is dead, the battery has a protective board that cuts off the power path. At…
Part Number: BQ24725A Other Parts Discussed in Thread: BQ24735 Hi team,
I found from BQ24725A datasheet that it is a Hybrid Power Boost Charge Controller, what does Hybrid mean? and Does it support reverse Boost mode? but I didn't find other detail from…
Part Number: BQ24725A Hello,
The BQ24725A buck charger is defined to accept Vin between 4.5v to 24v.
After reviewing its datasheet, I didn't find any peripheral requirement for working with a specific Vin.
Does that mean that in general the peripheral…
Part Number: BQ24725A Hello,
I am wondering if we can use BQ24725A or any other TI made ic can charge 3 to 4 sets of Smart Lithium-Ion Battery Pack. Preferably charging and discharging them sequentially. I also like to charge them by a single DC adapter…
Part Number: BQ24725A If there's any voltage drop in the path from the charger to the battery, will this charger sense the voltage after the drop, and compensate?
SRN and SRP seem related to current sense, not voltage sense, so i don't think they…
Part Number: BQ24725A Hi team,
my customer used BQ24725A to charge the battery. They use the adapter to charge the battery and the power of the adapter is 20V* 2A. They have set the charge current to 1.7A . And then they have connected an extra load…
Part Number: BQ24725A Hi,
We test the BQ24725A for the bettery charger and there are below issue:
1. During the testing process, when the battery is low in charge (with a battery voltage of around 9V), it was found that pq5&pq7 were damaged (mos ds short…