Part Number: BQ24725AEVM-710 Other Parts Discussed in Thread: TI-CHARGER-GUI , BQ24725A , USB2ANY , EV2400 Hi TI,
I download the SW app and try to run the setup application but got a pop up window "User account control" asking for admin user name and password…
Part Number: BQ24725AEVM-710 Other Parts Discussed in Thread: EV2400 Hi team,
good day,
Can you provide BQ24725EVM about MCU through IIC to the experimental board configuration routines.
Or about SMBus driver power management IC routines?
I look forward…
Part Number: BQ24725AEVM-710 Other Parts Discussed in Thread: BQ24725A Hello,
I am testing the BQ24725A-EVM with a SMBUS 1.1 compliant smart battery. I assumed the EVM would be plug and play with the smart battery, and automatically begin charging, but…
Part Number: BQ24725AEVM-710 Other Parts Discussed in Thread: BQ24725A
Hi,
I have been testing the BQ24725A-EVM with some of our smart batteries. Our smart batteries do not seem to have broadcast enabled, so we are using a host MCU to set the ChargingCurrent…
Part Number: BQ24725AEVM-710 Hi,
I test our EVM with R14, R15 unsoldered.
page 18 of the doc below:
And then I connect 2.6V from DC source directly to ACDET pin. And find that ACOK is low, which means that the device doesn't consider AC is okay. …
Part Number: BQ24725AEVM-710 I have an issue where the BQ24725AEVM-710 is not passing current from the supply to the load.
I first set the evaluation kit up according to Figure 2 in the User Guide and fail to get the correct voltages at the test points…
Part Number: BQ24725AEVM-710 Other Parts Discussed in Thread: BQ24725A , I have the BQ24725AEVM-710 and custom circuit board with the BQ24725A. On both circuits I am able to communicate to them via I2C, set and read the charge options, charge current, charge…
Part Number: BQ24725AEVM-710 Other Parts Discussed in Thread: BQ24725A Hi,
my customer is using this EVM to charge 2 cell battery with 9V input.
First time they set full voltage=8.2V, fast charge current =1A, the charge will suspend when battery voltage…
Part Number: BQ24725AEVM-710 Other Parts Discussed in Thread: BQ24725A Hello, I'd like to know if there is schematics and pcb Files compatibles to Altium Designer available in Texas Instruments website. If not, how can I get it? We are designing a battery…
Part Number: BQ24725AEVM-710 Other Parts Discussed in Thread: BQ24725A Hi,
I have BQ24725AEVM-710 evaluation board connected with a 4S1P smart battery. The evaluation board is also connected to a 20V and 3,3V power supply. When I measure voltages on the…