Other Parts Discussed in Thread: BQ24765 Hello,
we are using SMBus controlled battery charger BQ24765 in a BMS + Charger PCB of our design. BQ24765 is an integrated power mosfets, NMOS-NMOS, synchronous buck converter.
When we measure with the scope…
Other Parts Discussed in Thread: BQ24765 , BQ20Z40 Earlier this week I was using a bq24765 EVM to charge/discharge a 4S lipo battery through a bq20z40 EVM. I was able to charge and discharge the battery successfully and carefully put the work away. I…
Other Parts Discussed in Thread: BQ24765 , BQ20Z65 Good morning all,
Our 3S1P Li-ion battery pack is built around a BMS+charger PCB that uses BQ20Z65 as gas gauge and BQ24765 as charge controller. We set the CHGLED=1 so that during the charging phase…
Other Parts Discussed in Thread: BQ24765 Hello,
We are working with bq24765 battery charging controller. I want to drive pull ups of bq24765 ICs lines with external 3.3V supply (small LDO) and not from VREF of bq24765. This is because I want to…
Other Parts Discussed in Thread: BQ24765 From the BQ24765 Eval Module, is Q1 (BATFET) otherwise necessary if there is an alternative reverse polarity protection between the charger and the actual adapter.
Regards,
Pat
Other Parts Discussed in Thread: BQ24765 Hi there,
I'm working on the charger design using the BQ24765 and the BQ20Z95 on the the battery pack. I've 2 charging/discharging situation as below:
1. The CPU will be the host controller to control BQ24765…
Other Parts Discussed in Thread: BQ24765 , BQ20Z80 , BQ29312 , BQ29312A On page 26 of the datasheet for bq24765 it states that if the "battery voltage is still below 2.5V, a 220mA trickle charge current is applied." This would seem to only work with single…
Other Parts Discussed in Thread: BQ24765 Hello,
We would like to know that is it necessary that for correct operation of BQ24765, we need to build that circuit on 4-layer PCB only?
Or can the circuit be built on 2-layer PCB as well?
If we can…
Krunal, Wang
We are encountering the exact same issue where a charger (BQ24725) is holding the SDA line low after a long time operating, we have come up with a similar work around where we hold SCL low for >35 ms to reset the SDA line, as with your…