Part Number: BQ25100 Hi
I have a query need your help.
Does this chip have reverse voltage protection?
Does the red mark is reverse protection.
Thanks
Star
Part Number: BQ25100 Hi,
We have a design incorporating the BQ25100 to charge a small, 35mAh battery.
We have made about 80 units so far, with another 100 in progress. We are planning a small production run later this year of 5,000 units.
Our battery…
Part Number: BQ25100
Hi,
We are planning for a similar configuration described in below thread - TI Charger IC followed by PCM.
PCM will be in ship mode initially isolating battery from charger and rest of circuit.
Once charger is connected for the…
Part Number: BQ25100 Hello, I would need to know whether pin TS is a high impedance node looking into it such that I can also route the thermistor terminals to a fuel gauge which also uses this thermistor. Both the BQ25100YFPR and the FG would be simultaneously…
Part Number: BQ25100 Hello,
We want to use the BQ25100 in smartwatch and are worried about water ingress.
What happens if two pins are shorted, e.g. IN & VSS or OUT & TS or even IN & OUT?
Do we have an app-note on water protection?
Thank…
Part Number: BQ25100 Hi,
Is there are 3S version of BQ25100 for a Lithium-Ion Polymer battery?
We'd like to set up a external low current precharge to wake up the battery protection IC. The charger ICs that meet the rest of our requirements require…
Part Number: BQ51050B Other Parts Discussed in Thread: BQ25100 , Hi everyone,
I have integrated the BQ51050B into my system but now I realized that I need smaller charging current in the range of 20mA. Can I integrate the BQ51050B with the BQ25100 battery…
Part Number: BQ25100 Other Parts Discussed in Thread: BQ24105 Hello,
I want to charge a ML1220 coin cell battery but to be honest I am not sure if TI chipset can solve this issue...
TI chipset use 4.2V to charge lithium batteries and also minumun current…
Part Number: BQ25100 I'm using the BQ25100 to charge a small 12mAh LiOn-cell. We have until now produced more than 900 items and we find that some devices won't charge or stops being
able to charge after a few hours of use. Examining the external…
Part Number: BQ25100
Hello,
Customer wants to use 230mAh battery without NTC thermistor.
And wants to make enable and disable function by using TS pin.
Can BQ25100 be enabled and disabled by TS pin?
If possible, could you let me know how can make it…