Part Number: BQ25150EVM Other Parts Discussed in Thread: BQ25150 Hi, Am currently working on bq25150 battery controller, i have small issue with timers and watchdog timer, 1.Watchdog timer is getting reset, even though am disabling in CHARGERCTRL0 Register…
Part Number: BQ25150EVM Other Parts Discussed in Thread: BQ25150 , Hi
I have a question about register settings for BQ25150. I use the BQ25150EVM to power devices that consume about 50mA of current. I set a charging current of 70mA to the register, but the…
Part Number: BQ25150EVM Other Parts Discussed in Thread: BQSTUDIO , , BQ25155 Hi TI:
First time user of BQ25150EVM, fired up bqstudio, can't find it in its "supported targets" list.
What should I do? Thanks.
Part Number: BQ25150EVM Other Parts Discussed in Thread: BQ25150 Hi ,
We would like to measure current consumption from battery on our system.
I connected a KEITHLEY source meter with 4.0V output, and 1.05A current limit to replace Li-ion battery.
However…
Part Number: BQ25150EVM Other Parts Discussed in Thread: BQ25150 , EV2400 , BQSTUDIO
Hi,
1. Currently I am using BQ25150 TI EVM, but don't have battery.
2. Connected /CE pin to ground.
I want to do charging ON/OFF by I2C ICCTRL2(-> bit 0th) register…
Part Number: BQ25150EVM Hi ,
I want to generate wakeup1 & wakeup2 interrupt by /MR pin low.
Code logic :
1. mask all interrupts.
2. mask MRWAKE1_TIMEOUT & MRWAKE1_TIMEOUT
3. pull /MR line low & wait for this flag,
But flag not generate(interrupt…
Part Number: BQ25150EVM Hi ,
I have BQ25150EVM & 4.2 V, 220 mA battery.
1) when input current limit status bit was active ??
I have set -> 1. charging current : 100mA.
-> 2. input current limit : 100mA
2) I would like read battery charge current…
Part Number: BQ25150EVM Other Parts Discussed in Thread: BQSTUDIO Please be kind enough to email me the "Charger_1_00-bq25150.bqz" file as bqStudio (ver 1.3.86) doesn't have it.
Part Number: BQ25150EVM Other Parts Discussed in Thread: BQSTUDIO , EV2400 , It seems like no matter how I set the registers I am stuck at 10mA. I am using an EV2400 and BQStudio 1.3.86 with charger_1_00-bq25150.bqz as a configuration. Any suggestions?
…
Part Number: BQ25150EVM Other Parts Discussed in Thread: BQ25150 Hello,
BQ25150 has two LDOs :
- an always on Vdd 1.8v LDO <10mA.
- a 150mA LS/LDO which is active by default at 1.8v (e.g. without/before I2C use).
Question 1 : Why setup two LDO's active…