Part Number: BQ25170 Other Parts Discussed in Thread: TPS63070 , , BQ24170 , BQ25798 Tool/software: Hi teams,
I have a portable application that is evaluating the TI's solutions.
I draw a simple block diagram as below, could you please suggest the…
Part Number: BQ25170 Other Parts Discussed in Thread: BQ27220 Tool/software: Hi
I have used BQ27220 and BQ25170JDSGR for fuel guage and charger IC respectively in my system. I have connected BIN pin and TS pin of BQ27220 and BQ25170 IC respectively…
Part Number: BQ25170 Other Parts Discussed in Thread: BQ25180 , BQ24133 , BQ25185 , TPS63020 , TPS63060 , TPS63070 Tool/software: Hi, I need help in selecting a lipo battery charger. I have micro hydro generator with the following specs.
DC5V Technical…
Part Number: BQ25170 Tool/software: We have instances where the charger is always powered with 5 volts. The battery is connected to the charger and the device load. It appears that the charger may be only charging the battery when initially connected…
Part Number: BQ25170 Tool/software: Hi team,
Can you help to check below device's PN? Customer would like to design a low-cost charging PCB module. They find a old SCH which is suitable but they cannot confirm the PN. I check the roadmap also cannot…
Part Number: BQ25170 Tool/software: Dear TI Support,
I was wondering if you offered any Li-Ion Charging IC's for a 1-cell that can flash an LED during charge, and then stay on to indicate fully charged?
Regards, Kevin
Part Number: BQ25170 Tool/software: I have a schematic and layout completed using the Battery charger as mentioned above, and I request assistance in reviewing the schematic and layout.
Part Number: BQ25170 Tool/software: It's recommended to use 375 ohms for RISET or R34 in the schematic attached. However, the 375 ohm value is not available, and only the 374 ohm value is available.
Can I use 374 ohms instead of 375 ohms?