Part Number: BQ25170 Other Parts Discussed in Thread: TPS62808
Hello, I am using the BQ25170 to charge a 4.2V 1 cell Lipo battery. I have ordered 5 PCB’s and only 1 out of 5 charges my battery from 0V (When the voltage is cut off from the PCM). …
Part Number: BQ25170 Other Parts Discussed in Thread: TPS63070 , , BQ24170 , BQ25798 Tool/software: Hi teams,
I have a portable application that is evaluating the TI's solutions.
I draw a simple block diagram as below, could you please suggest the…
Part Number: BQ25170 Hi, I'm trying to charge a 3.7V lithium coin cell and I have the below circuit. I'm measuing 5.0V on the input of the charger and I have the battery voltage on the output but its not charging and the supply current is jumping up and…
Part Number: BQ25170 Other Parts Discussed in Thread: BQ27220 Tool/software: Hi
I have used BQ27220 and BQ25170JDSGR for fuel guage and charger IC respectively in my system. I have connected BIN pin and TS pin of BQ27220 and BQ25170 IC respectively…
Part Number: BQ25170 I am using BQ25170 to charge Li-Ion battery of 4.2V with 200mA charging current.Input is 5V from USBC
For setting the 200mA i will set the RISET to 1.5k. (RISET=300ohm*A/200mA).
During CC mode current will be 200mA,during trickle…
Part Number: BQ25170 Other Parts Discussed in Thread: BQ25180 , BQ24133 , BQ25185 , TPS63020 , TPS63060 , TPS63070 Tool/software: Hi, I need help in selecting a lipo battery charger. I have micro hydro generator with the following specs.
DC5V Technical…
Part Number: BQ25170J Hi Team,
I am using the BQ25170JDSGR in my design.
As per the datasheet, the output voltage (battery regulation voltage) is set using the VSET resistor. In my design, I am using a 24k ohm resistor , which should set the regulation…