Other Parts Discussed in Thread: BQ25180 Hi,
I designed a PCB which has BQ25180 IC. I am not sure about its INT pin. Firstly, i dont want to use INT pin but maybe, i can use it. My question is that should i connect 10kOhm-R25 or not? Or, what should…
Part Number: BQ25180 Hello Experts, I found a different comment about ship mode between datasheet and EVM user guide. I attached image as follows. Which one is correct? [datasheet] [EVM users guide] If customer set EN_RST_SHIP_1:0 of SHIP_RST Register…
Part Number: BQ25180 Hi Team,
my customer has 2.6A/100us on Vsys. I see in BQ25180, there is below spec, 2.5A/20ms but not sure if above will trigger OCP.
I also see bat_OCP can be disabled, if it's disabled, what will happen? Thanks.
BRs
…
Part Number: BQ25180 Other Parts Discussed in Thread: BQ24296 Hello Experts,
We are using BQ25180YBGR. I want to know current consumption in Ship mode and idle condition, When I press pushbutton(TS/MR) for 10 sec, current shown 10-30uA that means…
Part Number: BQ25180
Hello, Is it possible to properly recharge the following supercapacitor cell with the BQ25180? supercapacitor datasheet: https://br.mouser.com/datasheet/2/360/seiko_XH414HG-IV01E-1202874.pdf
The circuit we are planning to use…
Part Number: BQ25180 Other Parts Discussed in Thread: LM66100 Hi Team,
Our customer would like to connect two BQ25180 in parallel as shown in the schematic diagram below.
According to our customer,
I currently use BQ25180 for 1 cell battery…
Part Number: BQ25180 Other Parts Discussed in Thread: BQ25181 Hello,
We are using BQ25180 battery charger IC in our customer design. We have encountered problems in production, as many boards do not function at all when boards are coming from assembly…
Part Number: BQ25180 Hi,
We are using the BQ25180 charger in our system with a small 30mAh battery.
Our battery has an UVLO circuit that will essentially open a MOSFET if the cell voltage drops below 2.8V. At this point the charger will see a battery…
Part Number: BQ25180 I use BQ25180 in my prototype.
- I want to use its pushbutton functionality with both wake1 and wake2 press times (and of course long-press for ship mode)
- I do not use TS, so, as recommended by data sheet, I used pull down resistor…