Part Number: BQ25302 Hi all
My customer is working on a design with the BQ25302 and they have this question:
How do the TS and the REGN pins behave when USB is not connected ?
Are they tristate ? What is the internal circuit one has to consider…
Part Number: BQ25302 Hi team,
One of our customer will design wireless speaker. When they think they put two cells battery inside of the speaker. What is the pros/cons at series or parallels?
I think 2S1P needs cell balancing, but I don't know how…
Part Number: BQ25302 Hello guys,
One of my customers is evaluating BQ25302 on their own board for new products. They measured EMI level of the board. As the result, the EMI level was exceeded EMI level limit around 40Mhz and 200MHz. So they tried to…
Part Number: BQ25302 Hello All, I am working with the BQ25302 charger IC
when I power On the chip without the battery connected and VBUS=5V I can measure 1. around 0.8V on SW pin 2. 1V on PMID pin 3. REGN=0V After connecting the battery and Powering…
Part Number: BQ25302BQ25302EVM uses 1 uH MAPM0420LA1R0M-LF inductor that is difficult to source. I'm working with the customer on alternatives, preferably physically smaller. If you have suggestions, they would appreciated.
For 2A charge current what…
Part Number: BQ25302 Hello,
What values are recommended for the VBUS diode and the PFET when using the BQ25302 in an application with an external power path (2A maximum)?
Thank you and regards,
Alfred
Part Number: BQ25302 Hello
I've two questions about the external power path.
1. Is it necessary to add external power path for normal device such as mobile phone? the purpose is for better protection of battery? (prevent customers to charge and discharge…
Part Number: BQ25302 Hi all
My customer has a design with the BQ25302 and has three current limits selectable by the uC I/Os (schematic below).
100mA / 500mA / 1A
What happens in a low battery situation when the uC is not running ?
Consulting…
Part Number: BQ25302 Hi TI Team,
I have designed a charger circuit around BQ25302.
Schematic:
Observation:
The output voltage is set to 4.2V and a single-cell phone battery is connected
Input Voltage is kept at 5.4V DC
I am seeing charging…
Part Number: BQ25302 Hi all
My customer is working on a design with the BQ25302 and they have two questions:
For the PMID capacitor: on the simplified application schematic on page 1 of the datasheet they find 2.2uF while the datasheet specifies 10uF…