Part Number: BQ25306 Greetings:
We have been evaluating evaluation boards of BQ25306 (BMS005 Rev. A). We realized that there are two frequencies of LED's blinking periods when the power was turn on with a 2-cell battery: 1) 1Hz, 2) About 0.5Hz
…
Part Number: BQ25306EVM Hi all,
Now I am using BQ25306EVM for charging LiFePO4 battery.
the problem is that even I change charging current, charging time is almost same.
the condition is as below;
case1:
charging voltage : 3.6V (changed R5 to 455K)
…
Hello,
Thank you for reaching out via E2E. I do not observe this same behavior when testing charge termination on the BQ25306EVM with charge voltage set to 8.4V. Do you have the BAT pin connected closely to your battery terminal and are you measuring…
Hi Ann,
BQ25306 is a good candidate. The BAT pin is to be tied directly to the battery for remote sensing, so that true battery voltage is sensed, ignoring the trace loss, and increasing time spent in CC for faster charging. As it has a resistor divider…