Hello,
We have chargers that can buck DCDC charge and boost DCDC back to the input. However, for boost mode during battery only you will need to wait 30ms to boost back power.
If this is ok for you, I would recommend using either the BQ25895. This…
Audun,
A few questions on the next generation application:
1. What is the end equipment?
2. What are the specs on the battery planned to be used?
4. What is the max charging voltage and the charging current?
5. What kind of input? Will it be USB…
Jason,
1. When the BAT pin is connected to a real battery or a battery simulator, there will be trickle charge when VBAT is below VSHORT.
2. If the BAT pin is open, i.e. nothing is connected to the BAT pin, the BAT pin will have voltage only. Please…
So you will be adjusting the charge current manually through I2C, for each individual battery, correct?
What is the capacity of the batteries you are looking at?
And can you tell me a little more about the application? It is really to understand…
Part Number: BQ25600D We have a question for charge timer when low temp.
The setting value of the charge timer of BQ25600D is corrected to twice the time when low temperature is detected. For example, if the charge timer is set to 5 hours when room…
Hello Jasper,
The falling threshold of I2C active is the same as the falling depletion threshold, labeled VBAT_DPL_FALL.
Once I2C is active, it will remain so until the battery is thoroughly depleted below this threshold.
Regards,
Joel H