Part Number: BQ25713
Hi Team,
my customer find there is large possibility that BQ25713 cannot enter into OTG mode when in learn mode and need to quit learn mode first. Please kindly add your comments on if there is relationship with OTG and Learn Mode…
Hi hui,
hui peng said: 2. When PD25750 is the source, we support two types of PDO: 5V/3A and 9V/3A
Did you send the correct project? The one you sent has 15V and 20V PDOs
hui peng said: 5. We force the 4CC command to switch the role to sink, but it is not…
Part Number: BQ25713 Hi TI Teams,
We have some question about the applicatiion of the BQ25713, did the SYS output voltage can be set to fixed output? We need to set the output of SYS to fixed 4.4V.
If yes, how to set it.
If not, does the output voltage…
Part Number: TPS25750 Other Parts Discussed in Thread: BQ25713 , Hi,
We based our device power supply project on the TPS25750D (sink only) + BQ25713. The charger and Power Delivery (PD) are configured using EEPROM memory. At a charging voltage of 4.2V,…
Part Number: BQ25713 Hi
The customer design with BQ25713 of 2 string batteries. The test found that after over-discharge protection, the battery is trickle charged below 6.1V, with a current of 128MA.
It cannot be charged between 6.1V and 6.2V, and there…
Good Afternoon Dave,
We just released the newest TPS25751 GUI, and it includes support for the BQ25713.
USBCPD Application Customization Tool
Kind regards,
Conner Gillette
Part Number: BQ25713 We are working with an application where the default current reading resolution of the BQ25713 is on the low side.
We are using 100mOhm resistors for both sense resistors (RAC/RSR) and scaling the current readings back with factor…
Part Number: TPS25751 Other Parts Discussed in Thread: BQ25790 , BQ25713 , BQ25756 , , BQ25792 We learned from the datasheet of TPS25751 that the USBCPD Application Customization Tool only provides integrated control with BQ25756, BQ25790, and BQ25792. We…
Hi Field,
Field Tolson said: DaveNS_E2E_01FEB.bin
DRP can work when we use this binary, the connected sink device can stay charged.
Could you share the configuration of this bin file?
Thanks.
Best rehards,
Dave
Part Number: BQ25713 Hello.
My load operates at 5V and will draw maximum 5A from the supply.
Is it possible to fix this output using the USB-OTG to supply this power directly to my load, using a single cell 3.7V to supply the chip during the standalone…