Part Number: BQ25758 Tool/software: HI Sir,
BQ25758 pass inductor L1 "Table 7-1. Recommended Part Numbers for up-to 48-V EPR (5-A output): (continued)" show CMLB135T-100MS value: 10 μH, 22 mΩ, 10.5~13A
if i use 19.5V/15A input, is still can use the…
Part Number: BQ25758S Other Parts Discussed in Thread: BQ25758 , TPS25751 , TPS25730 Tool/software: Hi TI,
We are designing single cell battery chargers and there will be a total of 20 battery charging ICs in parallel with 0.5A output. We would like…
Part Number: BQ25758 Other Parts Discussed in Thread: BQ25756 , Tool/software: Hi team,
Customer ask what is the difference between BQ25756 and BQ25758,
Can you show the key differences of these two devices?
Is BQ25758 only can work with 14 cells…
Part Number: BQ25758 Other Parts Discussed in Thread: BQ25756 , TPS25751 , , TPS55289 Tool/software: When trying to configure the TPS25751 with the USBCPD application customization tool, the BQ25756 is presented as one of the battery chargers. I do not…
Part Number: BQ25758 Tool/software: Hi,
Recently I have started using BQ25758 which is available in Thunderbolt design, and configured IOUT_REG to trigger OCP at 1A current by programming IOUT_REG with value 0x0050.
When OCP occurs, I see that the…
Part Number: BQ25758 Tool/software: Hi Team,
Recently we are testing BQ25758 and found out that, it takes sometime for BQ25758 to ramp down from 48V to 5V.
We do have external discharge circuitry and when it is enabled VBUS on type-c connector discharge…
Part Number: BQ25758 Other Parts Discussed in Thread: BQ25756 , Tool/software: Hi, can you please revieuw the schematic of our design?
We know the inductor is just outside of the allowed range but we hope this will be fine since the DCR is withing spec…
Part Number: BQ25758 Tool/software: hi,
A my account needs a bidirectional converter with below spec. Can BQ25758 setting in buck-only mode(only two MOSFETs(Q1 & Q2) are used) support reverse mode?
Forward way: From input to output; input voltage…
Part Number: BQ25758 Other Parts Discussed in Thread: TPS25751 , , TPS25751EVM , BQ25756 , BQ25798 , BQ25713 , BQ25790 , BQ25792 , BQ25731 , BQ25756EVM Tool/software: How does the BQ26758 get set into reverse mode?
Presetting of registers? What method…