Part Number: BQ25798EVM Other Parts Discussed in Thread: BQSTUDIO , BQ25798 , Hi Jeff,
I am working on integrating BQ25798 in one of my device as a charger for a battery. I have tested and verified the working of BQ25798EVM hands on. I have a question…
Part Number: BQ25798EVM Other Parts Discussed in Thread: BQSTUDIO , BQ25798 Tool/software: Hi Tier
Could I use BQstudio to increase the charger current? How to do it.
And my customer found, EVM can use at 19V input, but when we change to 18.1 V…
Part Number: BQ25798EVM Other Parts Discussed in Thread: BQ25798 Hello, I am currently working with the BQ25798EVM development board and have encountered some unexpected behavior regarding the charge current under different input voltage conditions. I…
Part Number: BQ25798EVM Other Parts Discussed in Thread: BQ25798 , EV2400 VSYS was shorted to PGND resulting in a fast snap of a spark, the BQ25798 not outputting voltage/current after the fault was cleared, and the BQ25798 was also depowered and reset…
Part Number: BQ25798EVM Other Parts Discussed in Thread: BQ25798 Hello Jeff, We have observed following observation while performing the tests on BMS034A(EVAL BOARD BQ25798): -> When the Power is given from the Power Input Terminal & the Pull up connector…
Part Number: BQ25798EVM Hi Team,
My customer have been evaluating the BQ25798EVM and have noticed that it charges the battery at 1A by default according to Table 9-2
In their application the battery should be charged at 0.2C (700mA). They understood…
Part Number: BQ25798EVM Other Parts Discussed in Thread: BQ25792EVM Dear TI E2E Team,
I am writing to report some issues I encountered while using the BQ25798EVM development board. Specifically, I have encountered the following three problems:
…
Part Number: BQ25798EVM Other Parts Discussed in Thread: USB2ANY , BQ25798
Tool/software:
Hello! I created a copy board of the BQ25798EVM but instead of the LDO for PULLUP I placed a TI LMQ66420MC3RXBRQ1 Buck converter. The 2 problems are that:
…
Part Number: BQ25798EVM Hi Team,
My customer is facing issue with the battery charger BQ25798EVM eval kit.
When they connect an external USB charger it draws ~200mA with no load or battery connected to VSYS.
The IC’s temperature appears…
Part Number: BQ28Z620EVM-071 Other Parts Discussed in Thread: USB2ANY , EV2400 Tool/software: Is there a way for me to use the USBCPD application or BQ Studio through the USB2ANY device to configure and evaluate the gas gauge/cell balancer?