Part Number: BQ25882EVM-001 Dear all.
What is the function of D7 of EVM? When there is this diode, I think that a current flows through SYS from BAT when BATFET is off.
Best Regards, PAN-M
Part Number: BQ25882 Hi Team, BQ25882 is released now however I couldn't find user's guide for BQ25882EVM-001. Could you share the user's guide? http://www.ti.com/tool/bq25882evm-001 Best Regards, Yaita / Japan disty
Part Number: BQ25882 Hi,
The customer would like to evaluate BQ25882EVM-001 without host control, and also would like to set IINDPM to 500mA. I know that it has RLIM potentiometer (R5) to adjust IINDPM setting but the minimum setting is 1.094A at R5=10kohm…
Part Number: BQ25882 Hi,
It is written in the datasheet that an error when I set a termination current to 50mA is ±40%. Therefore, the upper side is 70mA. I measured termination current in two following environment.
1) BQ25882EVM-001 + 2cell Battery…