Part Number: BQ25890 Other Parts Discussed in Thread: , TPS25750 , BQ25792
I've looked over the datasheets for both BQ25890 and BQ25890H, but am having a hard time seeing what the difference is between the two. Clarification would be greatly appreciated…
Part Number: BQ25890 Hi
The customer design with BQ25890, REG12 read the current is normal in room temperature.
But in 5°C, the actual charging current is 200mA, REG12 reads 50mA; when the actual charging current is 115mA, REG12 reads 0mA.
Why the…
Part Number: BQ25895 Other Parts Discussed in Thread: BQ25890 , Hello TI,
What is the difference BQ25890 & BQ25895, which one is the recommended for new design.
Thanks,
Rahul.
Part Number: BQ25890
When the adapter is connected, we don't need to do any register writing to change the limit setting based on below description, right?
If it's detected as USB DCP, the current limit setting will be changed to 3.25A automatically…
Part Number: BQ25890 Hi all,
I am beginning for design battery charger. Can you confirm for me the battery charger BQ25890 can work with quick charge 2.0 adaptor or not.
And the document relate " MaxCharge TM Technology forHigh Input Voltage and Adjustable…
Part Number: BQ25890
1) REG03, what's the function of BAT_LOADEN?
2) What's the difference of REG06 BATLOWV vs REG03 SYS_MIN ?
3) REG09, what's the function purpose of current pulse control and PUMPX_UP/DN?
4) REG0D, what's the function of relative…
Part Number: BQ25890 Hi team,
OTG set max output current limit, now device limits the current and enters hiccup mode, not shut down. Can disable the hiccup mode by register in BQ25890?
Thanks
Lillian Liu
Part Number: BQ25890 Hi team,
OTG sets max output current limit, now it limits current and enters hiccup mode , but not shut down. Do we have a register that not show in the data sheet to disable the hiccup mode ?
Thanks!
Best regards
Lillian…
Part Number: BQ25890 I use BQ25890 as the charger chip, and use the BQ27441 as the voltameter.
I read the register of the two chips every 10 seconds , and plot the data into 5 graphs.
Since the graphs are large, they are attatched as a RAR below.…