Part Number: BQ25970EVM-893 Hi
I have some questions about the feature of SYNCOUT:
What is the benefit of SYNCOUT except reducing output voltage ripple?
Does the phase difference be held 90° by SYNCOUT between master BQ25970 and slave BQ25970…
Part Number: BQ25970EVM-893 Hi team,
The customer question is this
At the moment we are using BQ25971 and the efficiency of our device does not correspond to 97%? only 94%. Nevertheless, on the BQ25970EVM-893 board, the efficiency is 97%. I would…
Part Number: BQ25970EVM-893 Dear sir/madam,
I have purchase a BQ25970EVM-893 (Rev. B) and use bqstudio software to debug. The information I can found online is a user guild for Rev. A board. I don't know if it is the same for Rev. B board. When I…
Part Number: BQ25970EVM-893 Hi,
i got a quick question here, as shown in the bqstudio:
what's the difference between bq25970_S Field View and bq25970_M Field View?
Thanks.
Best regards
Mason
Part Number: BQ25970EVM-893 Hi members
I am looking for a readable schematic for the BQ25970EVM board. The schematic in the user guide is very pixalated and impossible to read.
Thanks in advance
Hello Vitaliy,
Unfortunately we do not sell that board anymore, we just have the design files.
We have the BQ25970EVM-893 which has 2 BQ25970s on board (no PD-Controller), as well as BQ25960H with 2 BQ25960HEVM and BQ25611D (no PD-Controller) and…
Part Number: BQ25970 Hello Sr,
As caption ,base on BQ25970EVM-893 I made a standalone board but it doens't work,none of regulate the input voltage how many volts there is no charge current delivered out from it even if up to 10-12Vdc on input, and the…
Part Number: BQ25970
Hello TI team,
now my customer consider BQ25970 for their product, i have some questions.
1. Can I use BQ25970 as standalone? because I saw the simplified application on page 1 of datasheet, there was also BQ2589x and PD controller…
Hi Ben,
Thanks for reaching us, you are right the TIDA-01582 is not a purchasable board. Most of customers is develop their own hardware with BQ25970 to start design, because varied MCU/AP and master charger are required. I would suggested to use…