Part Number: BQ27426EVM-738 I am doing the automated learning cycle. Battery capacity is 3500mAh, with a float voltage of 4.35V. After 22 hours of the learning cycle, the BQ Studios GUI is showing 99% and won't move on to the next step. The power supply…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: BQSTUDIO The battery information:
Battery design capacity:6000mAh
Battery Design Energy :2200mWh
Terminate Voltage: 3400mV
Questions:
Use BQStudio to do battery learning cycle , Skip charge and…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: EV2400 Hi
When using EV2400 and Battery Management Studio 1.3.101,unable to change the register configuration inside,
In the red box below, neither left-click nor right-click any options appear…
Part Number: BQ27426EVM-738 Dear Sir:
We use BQ27426EVM-738+BQ27000GDK for battery cycle learning,After the software is incorporated into the script, it can only be charged to 99% in the charging test, and the battery voltage is 3.4V lower than…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: BQ27426 , BQ24192 , BQSTUDIO , EV2400 Hi TI Team,
In our product for monitoring the battery we have used bq27426EVM-738 EVK and for charging the battery we have used bq24192EVM-021.
Both are connected…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: GPCCHEM , BQSTUDIO , BQ25155 Hey all,
i got today this failure during learning cycle. Error RUP_DIS / RDIS: not clear ! 7673.log_19.06.log
I already did the gpcchem and the batterycode 1325 was…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: BQSTUDIO , BQ27426 Hi
I met a bq27426EVM setup issue, i use GDK+BQstudio as test platform.
But i can't charge the battery through GDK, the EVM image shown below.
The red light(in the up right…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: BQSTUDIO , EV2400 , BQ27426 Hello,
I'm trying to get through the setup procedures documented in the user manual for the BQ27426EVM, and in bqStudio, there is no button for the Chemistry window…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: BQSTUDIO , BQ27426 Hello,
I'm trying to create a bqStudio project for the bq27426-EVM. I am charging a stand-alone Samsung 50E, Lithium 21700 battery, using the BQ24172EVM. The datasheet for…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: BQ27426 Hey all,
during testing BQ27426 with an connected RICOH R5443Z207PH (Protection IC) some failure was occurring that we didn't expect.
If we connected the Fuel Gauge with the Protection…