Part Number: BQ27441-G1 Other Parts Discussed in Thread: BQSTUDIO Hello,
We are using the bq27441-G1 fuel gauge ic for our battery monitoring system. below are the issue we are facing.
Trouble Setting Battery Capacity:: Sometimes, I can't set the right…
Part Number: BQ27441-G1 Other Parts Discussed in Thread: BQSTUDIO Hi
BQ27441 1-0055: rom_mode_gauge_dm_init: INITCOMP not set after 100 seconds
bq27441_battery.c
/*
* BQ27x00 battery driver
*
* Copyright (C) 2008 Rodolfo Giometti <giometti…
Part Number: BQ27441-G1 Other Parts Discussed in Thread: EV2400 , BQSTUDIO Hi,
I`m trying to start working with the battery fuel gauge and I have some questions:
this is my hardware and I'm connected to the device via EV2400:
1. I can't get accurate…
Part Number: BQ27441-G1 Other Parts Discussed in Thread: BOOSTXL-BATPAKMKII Dear TI Experts,
I have a BOOSTXL-BATPAKMKII Fuel Tank MKII Battery BoosterPack Plug-in Module and a Development Kit (MSP‑EXP432P401R). I used to plug them together and ran its…
Part Number: BQ27441-G1 Dear Expert
Our product encountered the following issues when using BQ27441: When the battery level is below 60%, unplug the battery, shut down and restart. After booting up, configure the power calibration file to BQ27441, and…
Part Number: BQ27441-G1 Other Parts Discussed in Thread: GPCCHEM , BQ28Z610 , BQSTUDIO Hello,
We're using the BQ27441DRZT-G1A fuel gauge in one of our products. We recently had to change our battery cell to a different manufacturer. I ran a relax, discharge…
Part Number: BQ27441-G1 Other Parts Discussed in Thread: BQ25890
Hi,
In my system, BQ25890 is used for charging and BQ27441 is used for battery gauge.
I use a 1900mAH battery. The BQ27441 init parameters are as follows:
The register data from BQ27441…
Part Number: BQ27441-G1 Hello,
I have been trying to find a solution to the problem for several days using the module, I cannot obtain the value of State of Charge and State of health of the battery but we are getting other parameters values. In the included…
Part Number: BQ27441-G1 The absolute max voltage for the Vpu (SDA, SCL, & GPOUT) is 6V but the recommended is 3.6V
Is it ok to pull up SDA and SCL to a LiPo 18650 cell (2.7-4.2V) even if it will go above 3.6V? Alternatively thinking of pulling up to…