Part Number: BQ27441EVM-G1A Other Parts Discussed in Thread: BQ27441-G1 , , BQSTUDIO , GPCCHEM , BQ27427 , BQ27426 Hello,
We are using BQ27441EVM-G1A to Monitor the SoC (State of Charge) and Voltage of 900 mAh battery, based on the battery specifications and the quick start gu…
Part Number: BQ27441EVM-G1A Other Parts Discussed in Thread: BQSTUDIO , GPCCHEM , BQ27426 , BQ27427 Using the bqStdio to poll the BQ27441 we observed large jumps in State of Charge during periods of load changes. One was from 57% to 43% and the other 56%…
Part Number: BQ27441-G1 Other Parts Discussed in Thread: BQSTUDIO Hi
BQ27441 1-0055: rom_mode_gauge_dm_init: INITCOMP not set after 100 seconds
bq27441_battery.c
/*
* BQ27x00 battery driver
*
* Copyright (C) 2008 Rodolfo Giometti <giometti…
Part Number: BQ27441EVM-G1A Other Parts Discussed in Thread: BQSTUDIO
Hello,
I'm using bqStudio to evaluate a BQ27441-G1A chip.
I'm comparing the data read with bqStudio with those read with my processor (STM32). I have exactly the same setup for…
Part Number: BQ27441EVM-G1A Is the Design Capacity what is written on the cell or the useable capacity from the cell. We are using the TPS65217C with a 1800mAh battery. However the cut off for the battery is 3.0V. The TPS65217C does not boost, so we are…
Part Number: BQ27441EVM-G1A Other Parts Discussed in Thread: BQ27411-G1 , GPCCHEM I have been working with fuel gauge IC BQ27411-G1.
We configured and found the battery percent. But after some time when we recheck with the battery percent.
It shown higher…
Part Number: BQ27441EVM-G1A Other Parts Discussed in Thread: BQ24075
Hi,
I am using BQ227441 in addition with BQ24075.i am using Bq27441 for the past 2 days and it worked fine for 2 days but suddenly BQ27441 stopped communicating with my controller which…
Part Number: BQ27441EVM-G1A Hello,
I utilize GPOUT to trigger a refresh on a set of display icons showing the SOC and whether the device is connected to power for charging...
When I remove charging power (and operating solely on battery) GPOUT pulses…
Part Number: BQ27441EVM-G1A Other Parts Discussed in Thread: BQ27441-G1 , BQ27441EVM-G1B Hi,I am trying to generate golden image using battery management studio version 1.3.86 and i am using BQ27441EVM-G1A evaulation boards along with EV2300
when i start…
Part Number: BQ27441EVM-G1A Hello,
Previsously, i wrote this post to know if there is any way to disable relax state using BQ27441-G1A.
following your suggestion(by setting the quit current as 0 to ignore relax state), the DSG flag is always at 0 even…