Part Number: BQ27520EVM Hi team,
The phenomenon:
1. The device cannot turn on and the battery is fully charged in a low temperature (10°C) environment.
2. The charge through the bq27520 is 0 and the temperature is 3 degrees.
3. Scope: Jiangxi province…
Your Ra Base value is extremely high. 307 equals 307*4 = 1228mOhm. With a load of 1494mA (avg I last run) and a full charge OCV of 4200mV, this would cause an immediate voltage drop to 4200mV - 1835mV = 2365mV, which is below Terminate Voltage + Delta…
Part Number: BQ27520EVM Other Parts Discussed in Thread: BQSTUDIO Hi,
I would need a help with chemistry id selection for my battery.
I use this battery https://www.gebattery.com.cn/product/showproduct.php?id=151 with 4.35V.
I did a relax-discharge-relax…
Part Number: BQ27520EVM Hollow.
The following is the learning cycle enumerated by the users guide of BQ27520EVM . These questions are also referenced in another document SLUA903–July 2018 -
Achieving The Successful Learning Cycle。
The original steps…
Part Number: BQ27520EVM Other Parts Discussed in Thread: BQSTUDIO , , BQ27520-G4 TI 技术支持您好,我已经准备好BQStudio 以及 EVM的环境,正在进行下一步的学习,有几个问题想咨询一下您:
Hi TI technical support, I have prepared the BQStudio and EVM environment, and are learning the next step. I have…
Other Parts Discussed in Thread: BQ27520EVM , GPCCHEM , BQSTUDIO Hello technical support:
At present, we have successfully learned the battery charge curve on the bq27520evm. Were also strictly according to the learning cycle document and get the dffs with…
Part Number: BQ27520EVM Other Parts Discussed in Thread: BQSTUDIO , , GPCCHEM
Hello,
I have been trying to do the learning cycle on a Panasonic NCR18650B using the BQ27520EVM and bqstudio.
Following the several guides available I am unsure what can still…
Part Number: BQ27520EVM
Hi,
we performed the measurement for our battery but didn't get a close matching chemical id. Before we plan sending the battery to you for evaluation could you check that the measurement has been done according to the TI guidelines…
Part Number: BQ27520EVM Hi,
I have been recently working on configuring a bq27520 chip in a project I am working on. I have been using the EVM to run chemical ID tests and learning cycle tests in an effort to generate a golden binary for programming the…
Part Number: BQ27520EVM Hi,
I am working on getting a bq27520 setup on a embedded device. I have completed the ChemID determination, Learning cycle, and Firmware Binary generation with an EVM. I have programmed the embedded devices with the updated firmware…