Part Number: BQ27531EVM Other Parts Discussed in Thread: BQSTUDIO Hello,
I am using bqStudio (v1.3.101).
I want to store the register of bq2419x in the flash of bq27531 and write it to POR automatically.
Press write_all to confirm that it has been written…
Part Number: BQ27531EVM Other Parts Discussed in Thread: BQ24192 Hi,
I'm trying to set the charging current of the BQ27531EVM to around 1 A. With a load of 500 mA on SYS, 169 ohm on ILIM, OTG disable and PSEL to ground, I only get a charging current…
LC_prevconfig_change_termV_tempcut_PS.log Hi Dominik,
I'm attempting to redo the learning cycle but I couldn't make it pass anymore. We have change the term volt to 2.8V as it was set too low before at 2.5V which is wrong. But for some reason, it's always…
Part Number: BQ27531EVM Other Parts Discussed in Thread: BQSTUDIO , BQ24192
Hi, Ti engineers:
I'm using the bq27531 fuel gauge + bq24192 Charger application, communication is done through bqstudio(V1.3.80) + EV2300(V3.1m).(communication tested well)…
Part Number: BQ27531EVM Hi,
I'm performing a learning cycle using the bq27531evm with a Panasonic Li-Ion 2000mah battery. In the spec, it is said that the "charge is terminated when charging current drops to 40mA". I then set the Data Flash Taper Current…
Part Number: BQ27531EVM Hi, I am trying to calibrate the temperature but the process in the software dont change de value I read.
Furthermore, I dont understand what does the parameters "Ext a Coef 1, Ext a Coef 2....."Ext type Coef 1, Ext type Coef 2…
Part Number: BQ27531EVM Other Parts Discussed in Thread: BQSTUDIO , , EV2400 , BQ27531-G1 , BQ24192 Hi,
I'm still new to battery charger/gauge so forgive me for asking a lot of questions. But this forum has been very helpful in accelerating my learning curve…
I am following slu595, to perform a learning cycle.
I am using a Varta 3.7V 2400mAh liPo battery.
I start with a discharged and fully relaxed battery that is measuring 3.0V open circuit.
Issue an IT_ENABLE
Charge to Full
Update Status goes from 0 to…
Other Parts Discussed in Thread: BQ27531EVM , BQ24192 , EV2400 Hello,
I recently ordered a BQ27531EVM and would like to know if fhis evaluation module that integrates a fuel gauge bq27531 and a battery charger bq24192 is compatible with the GDK (BQ27GDK000EVM…
Part Number: BQ24192 Other Parts Discussed in Thread: BQ27531EVM , , BQSTUDIO Hi,
I am doing development work on BQ27531EVM demo board ( Bq27531-g1 gauge and bq24192 charger). The battery that I'm using is Panasonic NCR18500A (1900mah).
While I'm doing the…