Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ35100 , BQ27Z561 , BQSTUDIO Tool/software: Primary cell gauges like the bq35100 have a newbattery() command to reset discharge and the like. Anything equivalent for the bq27z561?
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ27Z561 , BQSTUDIO Tool/software: Hello,
I am currently working with the BQ27Z561 and would like to configure it to enter both the Sleep and Deep Sleep modes.
I have followed the steps outlined…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ35100 , , BQ27Z561 Tool/software: What flashstream files are what? I have the following flashtream file output types: gm.fs
df.fs
bq.fs which is the firmware, which is the data flash, and…
Part Number: BQ27Z561-R2 Tool/software: Hello, Currently implementing a low power design utilizing the bq27z561-r2 guage. Due to power savings the hardware teams desires to disable the gauge while sleeping. The device will be sleep 99% of the time, with…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQSTUDIO Tool/software:
Hi
I set voltage time to 10s, deep sleep Voltage time to 20s, wake check time 5s using BQstudio,
and still saw current spikes (~2mA) every 1sec.
According to…
Part Number: BQ27Z561-R2 I'm looking to reduce complexity of my PCB stack-up. I would like to ground TS to allow me to get to the internal VSS pin next to it. Else I'm forced to use a blind micro via on the ground pad. I'm assuming this is OK as long…
Hello Priya,
Priya Joshi said: Given this constraint, is there any recommended way to stabilize or improve the accuracy of the SOC percentage under such varying load conditions?
Please reference section "4.81 Smoothing Engine"
Priya Joshi said:…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ27Z561 , GPCRB , BQSTUDIO Tool/software: 1round_verify.csv
round1_low_optimize_20250807-report.zip round2_low_optimize.zip
Hi,
Currently we have some issue with gauge BQ27z561 low temp…