Part Number: BQ3050 Other Parts Discussed in Thread: BQEVSW
Hello Team,
I have Discharge My battery completely , Below CUV threshold ( Just to Test ( Cell Voltage = 2500mV) ). Before CUV threshold RSOC was showing regularly on charge, but after this…
Part Number: BQ3050 Hello Team,
Battery Pack seems Charge Discharge perfectly in my case. Now , I want to Set RSOC = 100% when Cell voltage reaches to 4100mV while charging.
Hence , total Pack voltage would be not more than 16.4V for 2p4S config.…
Part Number: BQ3050EVM-001 Other Parts Discussed in Thread: BQ3050 , BQEVSW
Hello Team,
Is there any way where we can disconnect battery during RUNTIME ( i.e. no SMbus Communication , No Battery Output Voltage ( Pack+/Pack-) , No Current ) from…
Part Number: BQ3050 Other Parts Discussed in Thread: , BQEVSW , EV2400 Hello Team,
I see one strange battery / BMS voltage behavior here...
Battery have discharge upto RSOC=0% using Resistive Load of approx. 2A. Cell voltage go below 3190mV ( CUV…
Part Number: BQ3050 Other Parts Discussed in Thread: BQEVSW , , BQSTUDIO
Hello Team,
BatteryPack design is for 6900mAH / 14.4V using BQ3050.
I have done Current , Voltage and Temp calibration using BQEVSW software.
Current Calibration Done @ 1A…
Part Number: BQ3050 Other Parts Discussed in Thread: BQ24610 Hello everybody,
I 'm using BQ3050 for manager 3 Cells Li-ion battery. I use BQ24610 EVM as a charger for my battery.
When I connect Pack + and Pack - with BQ24610, I think battery will…
Part Number: BQ3050 Other Parts Discussed in Thread: EV2400 , BQSTUDIO Hi Team
It is first time customer uses BQ3050, and wants to read the config parameters of BQ3050, such as the overvoltage protection point, can it be read through the MCU software…
Part Number: BQ3050 Hello,
Although this BQ3050 4S6P LiFePO4 gas gauge is in full access, both charge and discharge fets are off.
I've been trying to force them "ON" by sending a write 0x0006 at address 0x46, but nothing happens. I've been performing…
Part Number: BQ3050 Hi,
I wanted to access the .senc file for bq3050. Therefore, I used the bootROM mode (0x0f00 command) in order to download the .senc file.
Following that I loose communication access to my battery after refreshing and cannot…
Thanks, Wyatt!
One last question, for bq3050, is there a way to deactivate "TDA Clear Volt" ?
E.g. "TDA Set Volt Time" can be disabled with setting to "0" and "FD Clear %" disabled with setting to "-1".
Is that possible somehow for "TDA Clear…