Part Number: BQ3050 Hello Is the SN8765 a complete analogue of the BQ3050 In particular, I'm interested in Data Flash Values for SN8765. I can not find the Technical Reference on SN8765 anywhere. I try to repair my home battery from the laptop in which…
Part Number: BQ3050 Other Parts Discussed in Thread: BQEVSW Hi,
one of our customers has inquired on how to read the data flash content of bq3050. Can you advise, which software they can use for this (bqEVSW?)? Does the software support unsealing the…
Part Number: BQ3050 Hi,
in one of our already released products we observed the battery pack entering Shutdown Mode without meeting all conditions defined.
We have set [SHUTV] = 1.
Regarding bq3050 Tech Ref it means Shutdown Mode is entered when…
Part Number: BQ3050 Dear Sir.There are BQ3050DBT and BQ3050DBTR two types are available at stores.I need to replace SN8765 IC .Which one is the correct one for SN8765 IC. Thanks.
Part Number: BQ3050 Hi team,
my customer wants to check following:
They have connected a chemical fuse on pin33, as depicted in the DS. They measure 132mV which translates into 490nA leakage. This is not stated in the DS so they ask following:
…
Part Number: BQ3050 Hi ,
We have desigened a battery with BQ3050. the depleted voltage threshold is 6V.
Recently, we find some batteries are enter depleted mode, and the voltage of pack is lower than 6V. We want to resume these batteries from depleted…
Part Number: BQ3050 Other Parts Discussed in Thread: GPCCEDV Hello,
I would like to be informed about the circumstances that are needed in order a successful learning cycle to be achieved (MaxError = 100% --> MaxError = 2%).
Is there any document…
Hello Onyx,
Thank you for your help.
Before I got your message, I exported the.gg file (text file) of a similar condition battery, then entered (write all) the values page by page into the dataflash of the brand new bq3050. And performed calibration…
Part Number: BQ3050 Hello,
Due to the lack of Information in the RTM about the meaning and the function of the ICC bit of the BatteryMode Register I would like you to answer us the following questions:
1) In page 74 says:
ICC: — This flag indicates…
Part Number: BQ3050 Other Parts Discussed in Thread: BQ40Z50-R1 , BQ40Z50-R2
Hello
My customer is using Battery pack using SN8765 ( Base device is bq3050 ) already in the market.
But they want to investigate SN8765 ( bq3050) themselves .
Anyway…