Hi EVAN
As i see the value range from 0~255(unit :Week), if i set the value to 0, what i will get ?.
And another question is : How to calculate the Max Chg Time and the Max Dsg Time?
[Learning Configuration(Monitoring)] Learning Frequen…
Part Number: BQ33100 Other Parts Discussed in Thread: BQEVSW , Hi
i meet some problems about the BQ33100 IC and BQEVSW issue. description as below :
1: Tool :bqEVSWSetup00.09.92_bq33100v0.15a
2: 3 different LOTs BQ33100 IC Only 1 LOT IC can communicate…
Part Number: BQ33100 1、Product : 5S super capacitor module(BQ33100),charge voltage 11.5v, design voltage 11.5V.
2、Function:Power backup
3、Design logistic:
- The default state required: CHGLVL1、LLEN and BQ33100_CHG are in Low Level condition.
After sending…
Part Number: BQ33100 Other Parts Discussed in Thread: EV2400 Hi Team,
I tried to make fault pin to drive high and to drive low, by sending SBS commands 0x0030 for making it HIGH and 0x0031 for making it LOW. But the pin remain unchanged. And the BQ33100…
Part Number: BQ33100 Dears:
About the detailed learning procedure,for my good understanding , please help me on below question:
1. Charge to V Learn Max Q1:if the value of V learn Max is a default value set in BQ33100, or the V learn Max is our product…
Part Number: BQ33100 Hi
Where and how i can read below informations ,tks !
1)Absolute State of Charge
2)Remaining Capacity
3)replace pack( a information or flag to inform user time to replace a health pack)
4)Microcode Update Reqd(a information or flag…
Hi,
I am struggling to recreate the error the capacitance and ESR error you are getting. Thank you for sending the .gg file, I have been using this since the .srec in unavailable. There is no update at the moment.
Regards,
Evan
Part Number: BQ33100 Hi team,
I am using BQ33100 in my design for a 5-cell configuration. For implementing the cell balancing feature i referred the application schematic given in the datasheet, and found that the mosfet used for cell balancing feature…
Part Number: BQ33100 Hi team,
I am using BQ33100 in my design. I referred the datasheet and found there are two grounds used in the reference schematic. Can anyone help in understanding why it is used. Also attaching snippet of the same.
Thanks & Regards…