Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: BQSTUDIO Hello,
The BQ35100EVM-795, that I'm working with, can not recognize the correct SOH value of the battery.
1) The circuit connection is as at the image below:
* All the jumpers are…
Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: BQSTUDIO Hi,
Used BQStudio version - 1.3.101
Unable to trigger New battery command after following steps -
1) Start Scan
2) Gauge Enable
3) Set security mode to Sealed
4) Set security mode…
Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: BQSTUDIO , BQ35100 Dear all,
I am using BQ35100EVM-795 EvalBoard in order to characterize the current absorptions of a PCB board supplied by a Li-SOCl2 battery by using BQSTUDIO.
The current…
Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: BQ35100 , BQSTUDIO , EV2400 Hello!
I use BMS with Windows Windows 10 Enterprise. When starting and selecting BQ35100 ist says it is not compatible with BQ35100.
When I go on it shows the device…
Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: BQSTUDIO , EV2400 Dear all,
I bought the BQ35100EVM-795 EvalBoard but I have had some troubles during its use.
As a matter of fact, once I have prepared the setup as shown on the User Guide SLUUBH7…
Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: EV2400 , BQSTUDIO , BQ35100
Hi,
My KMM designs ECU for agricultural vehicles.
Customer would like to try eval board BQ35100EVM-795.....but in the manual it is mentioned that it is necessary to…
Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: BQ35100 , MSP430FR5994 , BQSTUDIO , EV2400 I am using an MSP430FR5994 to read the voltage supplied to the BQ35100 via I2C using the command 0x08, as seen in the code below. The issue I am running…
Part Number: BQ35100EVM-795 Hi,
When I gauge a CR2032 battery using the State of Health (SOH) method, I initially inserted the battery into a CR2032 battery holder and connected it to the +Bat and -Bat terminals. I also connected a 165 Ohm resistor between…
Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: BQ35100 , BQSTUDIO I played with the Bq35100 and BQstudio.
I sealed the device accidentally, i pushed the SEAL push button. I remember the brand new chip was in Unsealed with FullAccess mode.…
Part Number: BQ35100EVM-795 Other Parts Discussed in Thread: BQ35100 , BQSTUDIO I played with the Bq35100 and BQstudio.
I have some misunderstanding about type of CC_offset' value and Board offset's unit. I see the data memory calibration page. …