Part Number: BQ40Z80 Other Parts Discussed in Thread: BQSTUDIO , EV2400 Tool/software: Trying it communicate with external MCU. Tried pressing wake up pin, were getting voltage at the output but not getting detected in the MCU. SMBus pins were pulled…
Part Number: BQ40Z80 Other Parts Discussed in Thread: BQSTUDIO , Tool/software: Hi,
I have a battery in CF. I try to delete it but impossible.
I have done a lot of charge/discharge cycles.
0% -> 100% -> 0% always wait for rest
100% -> 55% -> 100…
Part Number: BQ40Z80 Tool/software: Hello, In 4s BMS with Bq40z80 .It ws working normally before but when checked today the pack pin voltage is varying between 9.4 V to 12.2 V when the battery voltage was 16.45V. Why is this happening ?
Part Number: BQ40Z80 Tool/software: Hello TI Team,
We are using the BQ40Z80RSMR in our application and interfacing it with the iWave (SMARC IMX8QMAEC) S5 and S7 I2C lines. We have added 33 Ω, 1/16 W series termination resistors on these I2C lines near…
Other Parts Discussed in Thread: BQ40Z80 Tool/software: 1. Can we configure the GPIO pins of the BQ40z80 to perform our specific task like enable/disable of charge/discharge ? I want them to communicate with MCU based on some conditions it needs to be…
Part Number: BQ40Z80 Tool/software: Dear
BQ40Z80 is Register 0x0A reads the charging/discharging current, right? Right now, without it charged, the reading is 65368.
Other Parts Discussed in Thread: BQ40Z80 , BQ76942 , BQ34Z100 , BQ25756 Tool/software: Hi experts!
I'm looking for a standalone LiPo solution for a 6s1p battery pack. This should mean charger, BMS, and fuel gauge.
As of now, I'm planning on using…
Part Number: BQ40Z80 Other Parts Discussed in Thread: CSD18536KTT , CSD18540Q5B
Tool/software:
Hello, Despite the CSD1854Q5B suggested to use with BQ40z80, it has 29A discharge current. Wanted to have 60A discharge current MOSFET, currently with 29A…
Part Number: BQ40Z80 Other Parts Discussed in Thread: BQ7718 , BQ77207 Tool/software: Hello Anthony , Are there any changes in the input and the secondary protection of the bq40z80 schematic? It is for 6s, the EVM schematic was taken as the reference…
Part Number: BQ40Z80 Tool/software: During battery aging tests, it was observed that the Full Charge Capacity (FCC) gradually decreases as the number of aging cycles increases. However, the State of Health (SOH) behaves abnormally. Some batteries consistently…